<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: SC16IS741A Receiver time-out interrupt</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS741A-Receiver-time-out-interrupt/m-p/866392#M6817</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The time-out counter can only be reset at the center of each stop bit received or each time the receive FIFO is read.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately there are no application notes available or any other documents for the SC16IS741A other than the datasheet and packing and soldering information.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jan 2019 16:55:37 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2019-01-15T16:55:37Z</dc:date>
    <item>
      <title>SC16IS741A Receiver time-out interrupt</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS741A-Receiver-time-out-interrupt/m-p/866391#M6816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We&amp;nbsp;reset the&amp;nbsp;receiver time-out interrupt with a RX FIFO reset (write access to FCR[1] with value 1). This works fine for quite a while, but there is a chance to end up with a receiver time-out interrupt staying in pending mode. The /IRQ signals stays low. The interrupt source is verified with a read access to IIR register returning 0xCC. We considered the timing and respect the 2 x Tclk of XTAL1 requirement from datasheet. We use a external oscillator with 48MHz and 3.3V power supply. A new character received on UART RX creates a reset of the interrupt so does the read access to RHR.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anybody have another idea why the interrupt stays pending while reseting the RX FIFO?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any application note available about reset methods of each interrupt source similar to the description in 16C450 datasheet?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 13:06:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS741A-Receiver-time-out-interrupt/m-p/866391#M6816</guid>
      <dc:creator>andreas_pfaeffl</dc:creator>
      <dc:date>2019-01-10T13:06:59Z</dc:date>
    </item>
    <item>
      <title>Re: SC16IS741A Receiver time-out interrupt</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS741A-Receiver-time-out-interrupt/m-p/866392#M6817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The time-out counter can only be reset at the center of each stop bit received or each time the receive FIFO is read.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately there are no application notes available or any other documents for the SC16IS741A other than the datasheet and packing and soldering information.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 16:55:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS741A-Receiver-time-out-interrupt/m-p/866392#M6817</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-01-15T16:55:37Z</dc:date>
    </item>
  </channel>
</rss>