<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: PCA9615 Termination</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Termination/m-p/861565#M6771</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply. You are right to keep the voltage drop of R2 = 200mV for working normally. But the voltage over R2 depends on the differential output, not the R1. the Two R1s only provide bias.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Jan 2019 13:58:56 GMT</pubDate>
    <dc:creator>henryy</dc:creator>
    <dc:date>2019-01-21T13:58:56Z</dc:date>
    <item>
      <title>PCA9615 Termination</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Termination/m-p/861563#M6769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the datasheet, the output impedance is 100 Ohm differential. On page 9, it mentioned 'R2 is 120, R1 is 600, The parallel combination yields a termination of 100'. How this was calculated? Two R1s should be in series then parallel with R2. Then R1 should be 300 Ohm to yield a combination 100 Ohm. Did I miss anything? May I use R2=100Ohm and R1=10k to reduce the current?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2019 20:22:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Termination/m-p/861563#M6769</guid>
      <dc:creator>henryy</dc:creator>
      <dc:date>2019-01-08T20:22:22Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615 Termination</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Termination/m-p/861564#M6770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;No you can't use R1=10K. In the calculation you have to keep the voltage drop of R2=200mV to keep system working normally.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 01:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Termination/m-p/861564#M6770</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2019-01-09T01:22:29Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615 Termination</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Termination/m-p/861565#M6771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply. You are right to keep the voltage drop of R2 = 200mV for working normally. But the voltage over R2 depends on the differential output, not the R1. the Two R1s only provide bias.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2019 13:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Termination/m-p/861565#M6771</guid>
      <dc:creator>henryy</dc:creator>
      <dc:date>2019-01-21T13:58:56Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9615 Termination</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Termination/m-p/861566#M6772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;Same current flow into R2/R1s/R1s,there is voltage drop in R2 200mV,so also there are voltage drop in R1s.&lt;/P&gt;&lt;P&gt;If R1s value is large the voltage drop of R2 can't reach 200mV.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2019 06:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9615-Termination/m-p/861566#M6772</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2019-01-22T06:38:09Z</dc:date>
    </item>
  </channel>
</rss>