<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: Linux not parsing RedBoot partition table</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Linux-not-parsing-RedBoot-partition-table/m-p/155460#M677</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Try to make the rootfs.jffs2 out of LTIB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Run this command on ltib directory on PC:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;nbsp; mkfs.jffs2 -r rootfs -e 0x20000 -s 0x800 –n -o rootfs.jffs2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Use this created file "rootfs.jffs2"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Mar 2009 23:54:38 GMT</pubDate>
    <dc:creator>rogerio_silva</dc:creator>
    <dc:date>2009-03-31T23:54:38Z</dc:date>
    <item>
      <title>Linux not parsing RedBoot partition table</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Linux-not-parsing-RedBoot-partition-table/m-p/155459#M676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Hi,&lt;BR /&gt;&lt;BR /&gt;Im currently working on the imx31 - 3 stack board, and im trying to falsh the file system. I have already sucessfully loaded linux when using the NFS file system, but whenever i try to boot it with a flashed file system, it fails.&lt;BR /&gt;&lt;BR /&gt;I checked the log and it never tried to parse the RedBoot partition table, just create its own, generic partitions, then proceed to fail since it cant find any init scripts. I checked the options on the config file that ltib uses for configuring the kernel during compile time, and its checked to scan RedBoot partitions... am i missing some extra configs thatneed to&amp;nbsp; be done ?&lt;BR /&gt;&lt;BR /&gt;The booting log:&lt;BR /&gt;&lt;BR /&gt;Uncompressing Linux............................................................................................................ done, booting the kernel.&lt;BR /&gt;Linux version 2.6.19.2 (guilherme@RATM) (gcc version 4.1.1) #1 PREEMPT Mon May 12 10:53:19 BRT 2008&lt;BR /&gt;CPU: Some Random V6 Processor [4107b364] revision 4 (ARMv6TEJ), cr=00c5387f&lt;BR /&gt;Machine: Freescale MX31ADS&lt;BR /&gt;Memory policy: ECC disabled, Data cache writeback&lt;BR /&gt;CPU0: D VIPT write-back cache&lt;BR /&gt;CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets&lt;BR /&gt;CPU0: D cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets&lt;BR /&gt;Built 1 zonelists.&amp;nbsp; Total pages: 24384&lt;BR /&gt;Kernel command line: noinitrd console=ttymxc0,115200 root=/dev/mtdblock2 rootfstype=jffs2 rw ip=none&lt;BR /&gt;MXC IRQ initialized&lt;BR /&gt;PID hash table entries: 512 (order: 9, 2048 bytes)&lt;BR /&gt;Actual CLOCK_TICK_RATE is 16625000 Hz&lt;BR /&gt;Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)&lt;BR /&gt;Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)&lt;BR /&gt;Memory: 96MB = 96MB total&lt;BR /&gt;Memory: 93884KB available (2544K code, 519K data, 392K init)&lt;BR /&gt;Mount-cache hash table entries: 512&lt;BR /&gt;CPU: Testing write buffer coherency: ok&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;MXC GPIO hardware&lt;BR /&gt;system_rev is: 0x20&lt;BR /&gt;Clock input source is 26000000&lt;BR /&gt;assert standby signal *****************&lt;BR /&gt;L2 cache: WB&lt;BR /&gt;Using SDMA I.API&lt;BR /&gt;MXC DMA API initialized&lt;BR /&gt;otg_hs_suspend: reset isp1504&lt;BR /&gt;usb: Host 2 registered&lt;BR /&gt;usb: OTG HS Host registered&lt;BR /&gt;usb: OTG HS Gadget registered&lt;BR /&gt;CSPI: mxc_spi-0 probed&lt;BR /&gt;CSPI: mxc_spi-1 probed&lt;BR /&gt;MXC I2C driver&lt;BR /&gt;mc13783 Rev 3.3 FinVer 0 detected&lt;BR /&gt;Device spi2.2 probed&lt;BR /&gt;PMIC Character device: successfully loaded&lt;BR /&gt;PMIC RTC successfully probed&lt;BR /&gt;PMIC Power successfully probed&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;IP route cache hash table entries: 1024 (order: 0, 4096 bytes)&lt;BR /&gt;TCP established hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;TCP bind hash table entries: 2048 (order: 1, 8192 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 4096 bind 2048)&lt;BR /&gt;TCP reno registered&lt;BR /&gt;Low-Level PM Driver module loaded&lt;BR /&gt;DPTC driver module loaded&lt;BR /&gt;JFFS2 version 2.2. (NAND) (SUMMARY)&amp;nbsp; (C) 2001-2006 Red Hat, Inc.&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler anticipatory registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;mxc_sdc_fb mxc_sdc_fb.0: pixclock = 23980000l Hz&lt;BR /&gt;mxcfb: fb registered, using mode Epson-VGA&lt;BR /&gt;ch7024: TV encoder present: 45, read ret 0&lt;BR /&gt;Real TIme clock Driver v1.0&lt;BR /&gt;MXC WatchDog Driver 2.0&lt;BR /&gt;MXC Watchdog # 0 Timer: initial timeout 60 sec&lt;BR /&gt;Serial: MXC Internal UART driver&lt;BR /&gt;mxcintuart.0: ttymxc0 at MMIO 0x43f90000 (irq = 45) is a Freescale MXC&lt;BR /&gt;mxcintuart.1: ttymxc1 at MMIO 0x43f94000 (irq = 32) is a Freescale MXC&lt;BR /&gt;mxcintuart.2: ttymxc2 at MMIO 0x5000c000 (irq = 18) is a Freescale MXC&lt;BR /&gt;loop: loaded (max 8 devices)&lt;BR /&gt;IRQT_LOW set_irq_type ret = 0&lt;BR /&gt;Linux video capture interface: v2.00&lt;BR /&gt;MXC Video Output MXC Video Output.0: Registered device video16&lt;BR /&gt;MXC MTD nor Driver 2.0&lt;BR /&gt;mxc_nor_flash: probe of mxc_nor_flash.0 failed with error -5&lt;BR /&gt;block2mtd: version $Revision: 1.30 $&lt;BR /&gt;MXC MTD nand Driver 2.0&lt;BR /&gt;NAND device: Manufacturer ID: 0xec, Chip ID: 0xaa (Samsung NAND 256MiB 1,8V 8-bit)&lt;BR /&gt;Scanning device for bad blocks&lt;BR /&gt;Creating 6 MTD partitions on "NAND 256MiB 1,8V 8-bit":&lt;BR /&gt;0x00000000-0x00040000 : "Bootloader"&lt;BR /&gt;mtd: Giving out device 0 to Bootloader&lt;BR /&gt;0x00040000-0x00440000 : "Kernel"&lt;BR /&gt;mtd: Giving out device 1 to Kernel&lt;BR /&gt;0x00440000-0x08440000 : "Fla"&lt;BR /&gt;mtd: Giving out device 2 to Fla&lt;BR /&gt;0x08440000-0x08c40000 : "Flb"&lt;BR /&gt;mtd: Giving out device 3 to Flb&lt;BR /&gt;0x08c40000-0x0ea40000 : "Flc"&lt;BR /&gt;mtd: Giving out device 4 to Flc&lt;BR /&gt;0x0ea40000-0x10000000 : "Bootloader-priv"&lt;BR /&gt;mtd: Giving out device 5 to Bootloader-priv&lt;BR /&gt;MXC keypad loaded&lt;BR /&gt;input: mxckpd as /class/input/input0&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;IPU Post-filter loading&lt;BR /&gt;SSI module loaded successfully&lt;BR /&gt;PMIC Audio driver loading...&lt;BR /&gt;PMIC Battery successfully probed&lt;BR /&gt;Advanced Linux Sound Architecture Driver Version 1.0.13 (Tue Nov 28 14:07:24 2006 UTC).&lt;BR /&gt;Control ALSA component registered&lt;BR /&gt;ALSA device list:&lt;BR /&gt;&amp;nbsp; #0: MXC Freescale with PMIC&lt;BR /&gt;oprofile: using arm/arm11&lt;BR /&gt;TCP cubic registered&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;ieee80211: 802.11 data/management/control stack, git-1.1.13&lt;BR /&gt;ieee80211: Copyright (C) 2004-2005 Intel Corporation &amp;lt;jketreno@linux.intel.com&amp;gt;&lt;BR /&gt;Power Management for Freescale MX31&lt;BR /&gt;VFP support v0.3: implementor 41 architecture 1 part 20 variant b rev 2&lt;BR /&gt;input: mxc_ts as /class/input/input1&lt;BR /&gt;mxc input touchscreen loaded&lt;BR /&gt;VFS: Mounted root (jffs2 filesystem).&lt;BR /&gt;Freeing init memory: 392K&lt;BR /&gt;Warning: unable to open an initial console.&lt;BR /&gt;Kernel panic - not syncing: No init found.&amp;nbsp; Try passing init= option to kernel.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 May 2008 21:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Linux-not-parsing-RedBoot-partition-table/m-p/155459#M676</guid>
      <dc:creator>GMarchetti</dc:creator>
      <dc:date>2008-05-12T21:16:29Z</dc:date>
    </item>
    <item>
      <title>Re: Linux not parsing RedBoot partition table</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Linux-not-parsing-RedBoot-partition-table/m-p/155460#M677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Try to make the rootfs.jffs2 out of LTIB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Run this command on ltib directory on PC:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;nbsp; mkfs.jffs2 -r rootfs -e 0x20000 -s 0x800 –n -o rootfs.jffs2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Use this created file "rootfs.jffs2"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Mar 2009 23:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Linux-not-parsing-RedBoot-partition-table/m-p/155460#M677</guid>
      <dc:creator>rogerio_silva</dc:creator>
      <dc:date>2009-03-31T23:54:38Z</dc:date>
    </item>
  </channel>
</rss>