<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 [TJA1027] question about RXD</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1027-question-about-RXD/m-p/858399#M6725</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to connect TJA1027 LIN controller to a 3.3V interface on a FPGA. The datasheet shows the following application diagram. To work with a 3.3V FPGA interface, do I just need to add a pull the RXD signal (open-drain output) to 3.3V, not matter of the VBAT voltage on the other side of TJA1027? If this is correct, what pull-up resistance value should I use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything else I need to to on TXD and SLP_N signals (input)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!#&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="NXP_TJA-1027_LIN_diagram.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69698i1108152E2FD3E77A/image-size/large?v=v2&amp;amp;px=999" role="button" title="NXP_TJA-1027_LIN_diagram.jpg" alt="NXP_TJA-1027_LIN_diagram.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Feb 2019 20:26:37 GMT</pubDate>
    <dc:creator>bradlin1</dc:creator>
    <dc:date>2019-02-28T20:26:37Z</dc:date>
    <item>
      <title>[TJA1027] question about RXD</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1027-question-about-RXD/m-p/858399#M6725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to connect TJA1027 LIN controller to a 3.3V interface on a FPGA. The datasheet shows the following application diagram. To work with a 3.3V FPGA interface, do I just need to add a pull the RXD signal (open-drain output) to 3.3V, not matter of the VBAT voltage on the other side of TJA1027? If this is correct, what pull-up resistance value should I use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything else I need to to on TXD and SLP_N signals (input)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!#&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="NXP_TJA-1027_LIN_diagram.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69698i1108152E2FD3E77A/image-size/large?v=v2&amp;amp;px=999" role="button" title="NXP_TJA-1027_LIN_diagram.jpg" alt="NXP_TJA-1027_LIN_diagram.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Feb 2019 20:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1027-question-about-RXD/m-p/858399#M6725</guid>
      <dc:creator>bradlin1</dc:creator>
      <dc:date>2019-02-28T20:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: [TJA1027] question about RXD</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1027-question-about-RXD/m-p/858400#M6726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Please read about attached file page18-20 for your questions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Mar 2019 00:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1027-question-about-RXD/m-p/858400#M6726</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2019-03-01T00:22:25Z</dc:date>
    </item>
  </channel>
</rss>