<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problems with external Interrupt on MPC8360E MDS in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Problems-with-external-Interrupt-on-MPC8360E-MDS/m-p/155232#M666</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I think I found it. The Decrementer is also using the MSR[EE]. And when I enable the external interrupts the decrementer interrupt is captured too. And the reason for the reset is, that i've mapped the Flash memory to 0xFE00_000. So the Resetvector is @ 0xFEF0_0100, but i seems to be a problem for the MMU (or something else) if the Resetvector isn't @ 0xFF80_0000. So now I mapped the Flash to 0x0000_0000 and everything works fine.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Oct 2007 19:36:19 GMT</pubDate>
    <dc:creator>Timmo</dc:creator>
    <dc:date>2007-10-15T19:36:19Z</dc:date>
    <item>
      <title>Problems with external Interrupt on MPC8360E MDS</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problems-with-external-Interrupt-on-MPC8360E-MDS/m-p/155231#M665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello.&lt;BR /&gt;I'm trying to initialize the external Interrupt for the UART interface. But when I set the MSR[EE] bit to 1 I always get a Reset after 60 Seconds. The Watchdog is disabled (SWCRR = 0). The funny thing is, when I set the SIMSR_H and SIMSR_L to zero (therefore, no external interrupt should be recognized), I get an reset nevertheless. Is something connected to the external interrupt pin (inta) which is not decribed in the datasheet (not connected via IPIC)?&lt;BR /&gt;Another Problem is, when I setup the UART Controller for the &lt;I&gt;received data available interrupt&lt;/I&gt; (ERDAI) and after that I send a character to the controller, I get a reset too. Normally the Core should jump @ 0x0500, but the code which is placed there seems to be never executed.&lt;BR /&gt;I hope somebody can help me&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Oct 2007 16:38:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problems-with-external-Interrupt-on-MPC8360E-MDS/m-p/155231#M665</guid>
      <dc:creator>Timmo</dc:creator>
      <dc:date>2007-10-15T16:38:10Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with external Interrupt on MPC8360E MDS</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problems-with-external-Interrupt-on-MPC8360E-MDS/m-p/155232#M666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I think I found it. The Decrementer is also using the MSR[EE]. And when I enable the external interrupts the decrementer interrupt is captured too. And the reason for the reset is, that i've mapped the Flash memory to 0xFE00_000. So the Resetvector is @ 0xFEF0_0100, but i seems to be a problem for the MMU (or something else) if the Resetvector isn't @ 0xFF80_0000. So now I mapped the Flash to 0x0000_0000 and everything works fine.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Oct 2007 19:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problems-with-external-Interrupt-on-MPC8360E-MDS/m-p/155232#M666</guid>
      <dc:creator>Timmo</dc:creator>
      <dc:date>2007-10-15T19:36:19Z</dc:date>
    </item>
  </channel>
</rss>