<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: mc33908 reverse polarity</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/mc33908-reverse-polarity/m-p/832748#M6489</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tomas, the issue I have is that there must be some current flow into the pin prior to breakdown.&amp;nbsp; The pin clearly handles substantially greater voltages during the ISO 7637 tests (-100V and -150V or pulses 1 and 3a), so I'm trying to get a better understanding of the input architecture so I can defend our use case.&amp;nbsp; I have test data that shows this device survives repeated exposure to more than -14V but I don't have an engineering defense for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any insight you can provide is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Aug 2018 18:53:54 GMT</pubDate>
    <dc:creator>anzicek</dc:creator>
    <dc:date>2018-08-01T18:53:54Z</dc:date>
    <item>
      <title>mc33908 reverse polarity</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mc33908-reverse-polarity/m-p/832746#M6487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;#MC33908 -&amp;nbsp;Hello, I am curious what continuous reverse polarity the MC33908 #Vsense pin can withstand.&amp;nbsp; My implementation includes the external 5.1kOhm resistor, but the maximum ratings only show -14.0V as the max rating, no clamping voltage or current that the pin can withstand.&amp;nbsp; If a current were provided I could calculate.&amp;nbsp; There are also resistive dividers internal to the MC33908 on the Vsense pin, but the values of these are not given, again with the values of these, the -14V could be extrapolated to the input voltage with the 5.1k resistor.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Any help you can provide would be appreciated,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Thanks,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Josh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 16:07:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mc33908-reverse-polarity/m-p/832746#M6487</guid>
      <dc:creator>anzicek</dc:creator>
      <dc:date>2018-07-19T16:07:47Z</dc:date>
    </item>
    <item>
      <title>Re: mc33908 reverse polarity</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mc33908-reverse-polarity/m-p/832747#M6488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joshua,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First off, sorry for the delay in answering your question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The divider resistance value inside Vsense pin is MΩ level, so 5.1K has quite a little impact for Vsense pin voltage rating. -14V is maximum reverse voltage rating for both with or without 5.1K resistor&amp;nbsp;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it answers your question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2018 10:19:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mc33908-reverse-polarity/m-p/832747#M6488</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-08-01T10:19:03Z</dc:date>
    </item>
    <item>
      <title>Re: mc33908 reverse polarity</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/mc33908-reverse-polarity/m-p/832748#M6489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tomas, the issue I have is that there must be some current flow into the pin prior to breakdown.&amp;nbsp; The pin clearly handles substantially greater voltages during the ISO 7637 tests (-100V and -150V or pulses 1 and 3a), so I'm trying to get a better understanding of the input architecture so I can defend our use case.&amp;nbsp; I have test data that shows this device survives repeated exposure to more than -14V but I don't have an engineering defense for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any insight you can provide is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2018 18:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/mc33908-reverse-polarity/m-p/832748#M6489</guid>
      <dc:creator>anzicek</dc:creator>
      <dc:date>2018-08-01T18:53:54Z</dc:date>
    </item>
  </channel>
</rss>