<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: Load Switch ILim Pin issue</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Load-Switch-ILim-Pin-issue/m-p/830373#M6455</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For your schematic please make sure:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1: C136 1nf/16V or 25V(at least).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2:&lt;/SPAN&gt;&lt;SPAN style="font-size: 8.0pt;"&gt; Add external Schottky diode, NX5P3290 works well without it. To improve the lowest VBUS voltage during fast role swap, it is recommended to add a lower forward voltage diode, for example VF = 0.3 V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8.0pt;"&gt;3: Note the PCB layout, because of the CSP package with difficult solder. Suggest test the ILIM resistance with GND without power on.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Oct 2018 02:44:42 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2018-10-10T02:44:42Z</dc:date>
    <item>
      <title>Load Switch ILim Pin issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Load-Switch-ILim-Pin-issue/m-p/830370#M6452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using the NX5P3290UKZ load switch in our design.&lt;BR /&gt;The input to the switch is 5V at 3A(max) and output is limited to 5V at 1A using resistor of 49.9Kohm on ILim pin of switch. &lt;BR /&gt;We are seeing an issue that when we power ON the board the ILim pin of switch get shorted with ground(0ohm with respect to ground).&lt;BR /&gt;Kindly let us know your thoughts on the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Kiran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2018 04:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Load-Switch-ILim-Pin-issue/m-p/830370#M6452</guid>
      <dc:creator>kiran1</dc:creator>
      <dc:date>2018-10-08T04:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: Load Switch ILim Pin issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Load-Switch-ILim-Pin-issue/m-p/830371#M6453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you please show us your schematic?&lt;/P&gt;&lt;P&gt;Can you make sure that this is not your solder issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2018 02:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Load-Switch-ILim-Pin-issue/m-p/830371#M6453</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2018-10-09T02:45:43Z</dc:date>
    </item>
    <item>
      <title>Re: Load Switch ILim Pin issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Load-Switch-ILim-Pin-issue/m-p/830372#M6454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When we found that ILim pin got shorted with ground, we assumed load switch has gone bad and we replaced it with a new IC(Load switch). when we Powered it ON again we found a short on ILim pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find the Load switch schematics below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74113i1FF2698754261B48/image-size/large?v=v2&amp;amp;px=999" title="NXP_IMAGE.PNG" alt="NXP_IMAGE.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2018 04:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Load-Switch-ILim-Pin-issue/m-p/830372#M6454</guid>
      <dc:creator>kiran1</dc:creator>
      <dc:date>2018-10-09T04:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: Load Switch ILim Pin issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Load-Switch-ILim-Pin-issue/m-p/830373#M6455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For your schematic please make sure:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1: C136 1nf/16V or 25V(at least).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2:&lt;/SPAN&gt;&lt;SPAN style="font-size: 8.0pt;"&gt; Add external Schottky diode, NX5P3290 works well without it. To improve the lowest VBUS voltage during fast role swap, it is recommended to add a lower forward voltage diode, for example VF = 0.3 V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 8.0pt;"&gt;3: Note the PCB layout, because of the CSP package with difficult solder. Suggest test the ILIM resistance with GND without power on.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Oct 2018 02:44:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Load-Switch-ILim-Pin-issue/m-p/830373#M6455</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2018-10-10T02:44:42Z</dc:date>
    </item>
  </channel>
</rss>