<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCA9517DP-118 multi-master mode support in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9517DP-118-multi-master-mode-support/m-p/823549#M6350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am using the I2C repeater chip PCA9517DP-118 in my design. My application needs to read back voltage data from a voltage sequencer via I2C interface. I am using microprocessor and micro-controller in the module; I need both the microprocessor and micro-controller to read from voltage sequencer in multi-master mode. Microprocessor I2C interface is 2.5V standard, micro-controller I2C interface is 3.3V standard and slave device is also 3.3V standard. Microprocessor I2C level is translated to 3.3V by using the repeater PCA9517 (A side - 2.5V, B side - 3.3V) and then interfaced to slave device. Since micro-controller I2C interface is 3.3V standard it is directly interfaced to slave device. Therefore repeater B side is getting shorted to micro-controller I2C interface. Is there any issue with this method?. In the datasheet there is some static dc offset issue on the B side of repeater. Does this repeater supports multi-master mode on B side of repeater if B side is not tapped to B side of another repeater?. Refer the attached image for proposed architecture.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Hafiz&lt;span class="lia-inline-image-display-wrapper" image-alt="PCA9517DP-118.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67745i3EBA16B3066B5D74/image-size/large?v=v2&amp;amp;px=999" role="button" title="PCA9517DP-118.png" alt="PCA9517DP-118.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Aug 2018 10:11:34 GMT</pubDate>
    <dc:creator>hafiz_haja</dc:creator>
    <dc:date>2018-08-24T10:11:34Z</dc:date>
    <item>
      <title>PCA9517DP-118 multi-master mode support</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9517DP-118-multi-master-mode-support/m-p/823549#M6350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I am using the I2C repeater chip PCA9517DP-118 in my design. My application needs to read back voltage data from a voltage sequencer via I2C interface. I am using microprocessor and micro-controller in the module; I need both the microprocessor and micro-controller to read from voltage sequencer in multi-master mode. Microprocessor I2C interface is 2.5V standard, micro-controller I2C interface is 3.3V standard and slave device is also 3.3V standard. Microprocessor I2C level is translated to 3.3V by using the repeater PCA9517 (A side - 2.5V, B side - 3.3V) and then interfaced to slave device. Since micro-controller I2C interface is 3.3V standard it is directly interfaced to slave device. Therefore repeater B side is getting shorted to micro-controller I2C interface. Is there any issue with this method?. In the datasheet there is some static dc offset issue on the B side of repeater. Does this repeater supports multi-master mode on B side of repeater if B side is not tapped to B side of another repeater?. Refer the attached image for proposed architecture.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Hafiz&lt;span class="lia-inline-image-display-wrapper" image-alt="PCA9517DP-118.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67745i3EBA16B3066B5D74/image-size/large?v=v2&amp;amp;px=999" role="button" title="PCA9517DP-118.png" alt="PCA9517DP-118.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2018 10:11:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9517DP-118-multi-master-mode-support/m-p/823549#M6350</guid>
      <dc:creator>hafiz_haja</dc:creator>
      <dc:date>2018-08-24T10:11:34Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9517DP-118 multi-master mode support</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9517DP-118-multi-master-mode-support/m-p/823550#M6351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hafiz Haja,&lt;/P&gt;&lt;P&gt;There is no problem with your dessign, since the PCA9517 is multi-master capable, the DC off set at B side wont be a problem, just make sure to be at or lower than 0.4V for arbitration or clock stretching to be transmitted to A side.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aldo&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2018 15:02:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9517DP-118-multi-master-mode-support/m-p/823550#M6351</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2018-08-27T15:02:47Z</dc:date>
    </item>
  </channel>
</rss>