<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: LDMOS degradation issue</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/LDMOS-degradation-issue/m-p/821877#M6330</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The gradual device degradation can be a consequence of repeated avalanche condition caused by the drain over-voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Typical reasons of over-voltage is high VSWR or transient spikes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case of RF pulse signal, the over-voltage can be caused by RF envelope oscillation at the RF pulse edges because of low frequency resonance of RF choke inductance and output capacitance of the transistor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Typical recommendation is to decrease slew rate of input signal RF envelope &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Dec 2018 10:53:56 GMT</pubDate>
    <dc:creator>LPP</dc:creator>
    <dc:date>2018-12-03T10:53:56Z</dc:date>
    <item>
      <title>LDMOS degradation issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LDMOS-degradation-issue/m-p/821876#M6329</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to ask a query regarding the performance of NXP LDMOS Power Transistor part No. mmrf1312H. I am facing the reliability issue of the said device. I successfully achieved the desired parameters from the device which are stated below as:&lt;/P&gt;&lt;P&gt;RF Output Power Level (peak) = 60dBm (1000W)&lt;BR /&gt;Efficiency= 55%&lt;BR /&gt;Gain = 16.5 dB&lt;/P&gt;&lt;P&gt;Operating parameters are given below:&lt;/P&gt;&lt;P&gt;VDD=50V &lt;BR /&gt;(supply was providing +30V, DC-DC converter was used to get +50V) &lt;BR /&gt;Quiescent current =100mA (VGS=1.94V)&lt;BR /&gt;Pulse Width = 256usec&lt;BR /&gt;PRF=400Hz&lt;BR /&gt;Duty Cycle= 10%&lt;BR /&gt;Operating Temperature = 25 degree centigrade&lt;/P&gt;&lt;P&gt;After successfully achieved the desired parameters, i turned the device on for longer span to check the reliability of the device, but after 40 minutes suddenly the device output power drops to 200W, i turned off the power supply and did check the device via DMM. The gate terminal of the device showed short circuit.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Again i performed the test by installing the new device into the circuit. it successfully produced an output power of around 1000W but after 70 mins, it got damaged too.&lt;/P&gt;&lt;P&gt;I tested 8 devices, all of them got damaged gradually. Some devices were moderately failed and some were completely failed. Their life time span was 40mins, 70mins, 200mins, 30mins, 50mins, 120mins, 80mins, 20mins respectively.&lt;/P&gt;&lt;P&gt;Please note that the following mentioned precautions were taken while performing the test.&lt;/P&gt;&lt;P&gt;RF Input Power level was under 20W as provided in the datasheet.&lt;BR /&gt;Isolator was inserted at the output line of transistor to protect the device from high VSWR.&lt;BR /&gt;Heat sink temperature was continuously monitored, it was around 45 degree at the time when device got damaged.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am so confused, what could be the reason, please help me, i shall be very thankful to you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Nov 2018 07:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LDMOS-degradation-issue/m-p/821876#M6329</guid>
      <dc:creator>hassanferoze073</dc:creator>
      <dc:date>2018-11-30T07:11:18Z</dc:date>
    </item>
    <item>
      <title>Re: LDMOS degradation issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LDMOS-degradation-issue/m-p/821877#M6330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The gradual device degradation can be a consequence of repeated avalanche condition caused by the drain over-voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Typical reasons of over-voltage is high VSWR or transient spikes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case of RF pulse signal, the over-voltage can be caused by RF envelope oscillation at the RF pulse edges because of low frequency resonance of RF choke inductance and output capacitance of the transistor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Typical recommendation is to decrease slew rate of input signal RF envelope &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Dec 2018 10:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LDMOS-degradation-issue/m-p/821877#M6330</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2018-12-03T10:53:56Z</dc:date>
    </item>
  </channel>
</rss>