<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: A2I25D025</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/A2I25D025/m-p/820130#M6319</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;thank you for the helpful information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Holger&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jun 2018 12:52:29 GMT</pubDate>
    <dc:creator>he1</dc:creator>
    <dc:date>2018-06-28T12:52:29Z</dc:date>
    <item>
      <title>A2I25D025</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/A2I25D025/m-p/820128#M6317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the A2I25D025 data sheet there are two different PCB layouts "production test circuit" and "characterization test circuit". In the first one the RFout pins are connected to VDD in the second they are not. Does anybody know what is correct?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Holger&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 09:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/A2I25D025/m-p/820128#M6317</guid>
      <dc:creator>he1</dc:creator>
      <dc:date>2018-06-26T09:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: A2I25D025</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/A2I25D025/m-p/820129#M6318</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The pins 17 (VBWA) and 16 (RFOUT1) are DC connected internally. This&amp;nbsp; explains the circuit on Figure 4 (VDD2A is connected to VBWA).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VBW leads are connected to an internal RF cold spot in the internal output matching circuit.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;The characterization reference design utilizes these leads to provide the VDD stage two drain bias, and the leads are RF decoupled to &lt;BR /&gt;ground with some bias caps.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;The purpose of this bias structure is to reduce the effective lead inductance between the die and the external bias decoupling caps to &lt;BR /&gt;improve the VBW capability of the device. Most other RF IC parts of this size, MW7IC2725N have VBW rating in the 90 MHz range. With this &lt;BR /&gt;alternative biasing structure, the VBW is 170 Mhz.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;There is some RF power loss thru these leads and if a wide VBW is not required, then the part can be biased in a normal manner thru an RF &lt;BR /&gt;choke on the drain lead and achieve better RF performance.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;It is a designer’s option, wider VBW or better RF.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 13:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/A2I25D025/m-p/820129#M6318</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2018-06-27T13:36:16Z</dc:date>
    </item>
    <item>
      <title>Re: A2I25D025</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/A2I25D025/m-p/820130#M6319</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;thank you for the helpful information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Holger&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jun 2018 12:52:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/A2I25D025/m-p/820130#M6319</guid>
      <dc:creator>he1</dc:creator>
      <dc:date>2018-06-28T12:52:29Z</dc:date>
    </item>
  </channel>
</rss>