<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic pcf85263a not counting in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/pcf85263a-not-counting/m-p/812253#M6238</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the PCF85263A RTC with BeagleBone Black board running linux: debian jessie. I have connected it to my i2c-1 line and am able to see it at address 0x51. I can do i2cdump and see registers values. I'm trying to get it to start by following the steps in datasheet section 8.2.6:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Set STOP bit to HIGH 1 in register 2E&lt;/P&gt;&lt;P&gt;- Clear the prescaler by writing 0xA4 to register 0x2F ( i do not see confirmation on this register when I try to read it back but I assume it works since when I write 0x2C in this register it resets all registers to Default values)&lt;/P&gt;&lt;P&gt;- Set time registers&lt;/P&gt;&lt;P&gt;- Set the STOP bit to LOW 0 in register 2E (according to datasheet time is supposed to start counting from this point)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I do the rest of the steps and set STOP bit back to 0 it do not see the values in the registers increment at all? what am I missing? I'm not using any drivers for this currently since I could only find drivers for pcf8563 in my 4.4-ti kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also what about the OS bit in the register 0x01 (100th second)? It mentions that I should clear it so the oscillator is running but when I try to set it to 0 it retains its prev value of 1(register value of 0x80). How can I clear it? Is this what is causing the clock not to increment?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What should I do to get this running properly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Nov 2018 21:09:16 GMT</pubDate>
    <dc:creator>ghaddama</dc:creator>
    <dc:date>2018-11-07T21:09:16Z</dc:date>
    <item>
      <title>pcf85263a not counting</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/pcf85263a-not-counting/m-p/812253#M6238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the PCF85263A RTC with BeagleBone Black board running linux: debian jessie. I have connected it to my i2c-1 line and am able to see it at address 0x51. I can do i2cdump and see registers values. I'm trying to get it to start by following the steps in datasheet section 8.2.6:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Set STOP bit to HIGH 1 in register 2E&lt;/P&gt;&lt;P&gt;- Clear the prescaler by writing 0xA4 to register 0x2F ( i do not see confirmation on this register when I try to read it back but I assume it works since when I write 0x2C in this register it resets all registers to Default values)&lt;/P&gt;&lt;P&gt;- Set time registers&lt;/P&gt;&lt;P&gt;- Set the STOP bit to LOW 0 in register 2E (according to datasheet time is supposed to start counting from this point)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I do the rest of the steps and set STOP bit back to 0 it do not see the values in the registers increment at all? what am I missing? I'm not using any drivers for this currently since I could only find drivers for pcf8563 in my 4.4-ti kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also what about the OS bit in the register 0x01 (100th second)? It mentions that I should clear it so the oscillator is running but when I try to set it to 0 it retains its prev value of 1(register value of 0x80). How can I clear it? Is this what is causing the clock not to increment?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What should I do to get this running properly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Nov 2018 21:09:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/pcf85263a-not-counting/m-p/812253#M6238</guid>
      <dc:creator>ghaddama</dc:creator>
      <dc:date>2018-11-07T21:09:16Z</dc:date>
    </item>
  </channel>
</rss>