<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Productsのトピックsc16is750 horrid TX output when RX left floating</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/sc16is750-horrid-TX-output-when-RX-left-floating/m-p/807289#M6206</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the RX pin need to be pulled up or pulled down when not using? My guess for TX not&amp;nbsp;producing a signal greater than 600mV peak to peak and having a nasty slope down (like a cap discharge) on the high of the "square wave" is because I left the RX pin floating. This is the only thing&amp;nbsp;I did differently from my other sc16is750 which is also on the board and works fine. We are using the chip as just a transmitter.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jun 2018 14:32:43 GMT</pubDate>
    <dc:creator>jtwhissel</dc:creator>
    <dc:date>2018-06-21T14:32:43Z</dc:date>
    <item>
      <title>sc16is750 horrid TX output when RX left floating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/sc16is750-horrid-TX-output-when-RX-left-floating/m-p/807289#M6206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the RX pin need to be pulled up or pulled down when not using? My guess for TX not&amp;nbsp;producing a signal greater than 600mV peak to peak and having a nasty slope down (like a cap discharge) on the high of the "square wave" is because I left the RX pin floating. This is the only thing&amp;nbsp;I did differently from my other sc16is750 which is also on the board and works fine. We are using the chip as just a transmitter.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2018 14:32:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/sc16is750-horrid-TX-output-when-RX-left-floating/m-p/807289#M6206</guid>
      <dc:creator>jtwhissel</dc:creator>
      <dc:date>2018-06-21T14:32:43Z</dc:date>
    </item>
    <item>
      <title>Re: sc16is750 horrid TX output when RX left floating</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/sc16is750-horrid-TX-output-when-RX-left-floating/m-p/807290#M6207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Whissel &lt;BR /&gt;Did you try disabling the Rx when not using it, writing a 1 to RXDISABLE to the Extra Features Control Register (ECFR), &lt;BR /&gt;if you did a pull-up resistor should work, around 10k.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 16:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/sc16is750-horrid-TX-output-when-RX-left-floating/m-p/807290#M6207</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2018-06-26T16:25:03Z</dc:date>
    </item>
  </channel>
</rss>