<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 74LVC2G125 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/74LVC2G125/m-p/785312#M5984</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Unfortunately 74LVC2G125 had already transfer into NEXPERIA,you can contact with them for more technical support!&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nexperia.com/products/logic/asynchronous-interface-logic/buffers-inverters-drivers/series/74LVC2G125.html" title="https://www.nexperia.com/products/logic/asynchronous-interface-logic/buffers-inverters-drivers/series/74LVC2G125.html"&gt;74LVC2G125 - Dual bus buffer/line driver; 3-state | Nexperia&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Nov 2018 04:50:21 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2018-11-22T04:50:21Z</dc:date>
    <item>
      <title>74LVC2G125</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/74LVC2G125/m-p/785311#M5983</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Data Sheet says:&lt;/P&gt;&lt;P&gt;This device is fully specified for partial power-down applications using IOFF. The IOFF circuitry&lt;BR /&gt;disables the output, preventing a damaging backflow current through the device when it is powered&lt;BR /&gt;down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The similar device SN74LVC2G125 from TI says:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This device is fully specified for partial-power-down&lt;BR /&gt;applications using Ioff. The Ioff circuitry disables the&lt;BR /&gt;outputs, preventing damaging current backflow&lt;BR /&gt;through the device when it is powered down.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ioff Supports Live Insertion, Partial-Power-Down&lt;BR /&gt;Mode, and Back-Drive Protection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Partial Power Down (Ioff):&lt;BR /&gt;The inputs and outputs for this device enter a high impedance state when the supply voltage is 0 V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Logically, NXP 74LVC2G125 is the same&amp;nbsp;as TI SN74LVC2G125,&amp;nbsp;&lt;/P&gt;&lt;P&gt;but I would like to make sure whether the input is in high impedance or not while Vcc=0 for NXP 74LVC2G125.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 15:13:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/74LVC2G125/m-p/785311#M5983</guid>
      <dc:creator>junboyi</dc:creator>
      <dc:date>2018-11-21T15:13:49Z</dc:date>
    </item>
    <item>
      <title>Re: 74LVC2G125</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/74LVC2G125/m-p/785312#M5984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Unfortunately 74LVC2G125 had already transfer into NEXPERIA,you can contact with them for more technical support!&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nexperia.com/products/logic/asynchronous-interface-logic/buffers-inverters-drivers/series/74LVC2G125.html" title="https://www.nexperia.com/products/logic/asynchronous-interface-logic/buffers-inverters-drivers/series/74LVC2G125.html"&gt;74LVC2G125 - Dual bus buffer/line driver; 3-state | Nexperia&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Nov 2018 04:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/74LVC2G125/m-p/785312#M5984</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2018-11-22T04:50:21Z</dc:date>
    </item>
  </channel>
</rss>