<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NVT2008BQ LEVEL TRANSLATOR OPERATION in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/NVT2008BQ-LEVEL-TRANSLATOR-OPERATION/m-p/762823#M5763</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the level translator IC -NVT2008BQ in our design.But in our application , same voltage will be used at the both sides of the level translator in certain times (VADJ_1V8,it can be 1.2V or 1.8V). In datasheet its mentioned like "The applied voltages at Vref(A) and Vpu(D) should be such that Vref(B) is at least 1 V higher than Vref(A) for best translator operation." Could you please confirm whether this level translator can work with same voltages on both sides(Its not clear from the datasheet page.9) ? Or any other modification required for the following design which is attached with this? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Jun 2018 09:04:47 GMT</pubDate>
    <dc:creator>bijumohankc</dc:creator>
    <dc:date>2018-06-08T09:04:47Z</dc:date>
    <item>
      <title>NVT2008BQ LEVEL TRANSLATOR OPERATION</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NVT2008BQ-LEVEL-TRANSLATOR-OPERATION/m-p/762823#M5763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the level translator IC -NVT2008BQ in our design.But in our application , same voltage will be used at the both sides of the level translator in certain times (VADJ_1V8,it can be 1.2V or 1.8V). In datasheet its mentioned like "The applied voltages at Vref(A) and Vpu(D) should be such that Vref(B) is at least 1 V higher than Vref(A) for best translator operation." Could you please confirm whether this level translator can work with same voltages on both sides(Its not clear from the datasheet page.9) ? Or any other modification required for the following design which is attached with this? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2018 09:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NVT2008BQ-LEVEL-TRANSLATOR-OPERATION/m-p/762823#M5763</guid>
      <dc:creator>bijumohankc</dc:creator>
      <dc:date>2018-06-08T09:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: NVT2008BQ LEVEL TRANSLATOR OPERATION</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NVT2008BQ-LEVEL-TRANSLATOR-OPERATION/m-p/762824#M5764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This question is being solved internally (Case #00166169).&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2018 10:27:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NVT2008BQ-LEVEL-TRANSLATOR-OPERATION/m-p/762824#M5764</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-06-11T10:27:27Z</dc:date>
    </item>
  </channel>
</rss>