<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックI2C range extender PCA9507</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754858#M5704</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two questions regarding PCA9507, I2C bus extender.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Accoding to datasheet, distance, using this IC, is limited 1400pF or 18m&amp;nbsp;on port A.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My questions now are:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;1. Is this limit, 18m, having PCA9507 on one side only or it has to be on both sides, if we talk about point-to-point?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;2. If I have PCA9507 on both sides, is it OK to have port A towards each other, since there are rise time accelerators?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am asking this since our board has HDMI input and output ports.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answers.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Enjoy the rest of the weekend.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rok&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 31 Mar 2018 17:30:03 GMT</pubDate>
    <dc:creator>roklipar</dc:creator>
    <dc:date>2018-03-31T17:30:03Z</dc:date>
    <item>
      <title>I2C range extender PCA9507</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754858#M5704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two questions regarding PCA9507, I2C bus extender.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Accoding to datasheet, distance, using this IC, is limited 1400pF or 18m&amp;nbsp;on port A.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My questions now are:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;1. Is this limit, 18m, having PCA9507 on one side only or it has to be on both sides, if we talk about point-to-point?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;2. If I have PCA9507 on both sides, is it OK to have port A towards each other, since there are rise time accelerators?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am asking this since our board has HDMI input and output ports.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answers.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Enjoy the rest of the weekend.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rok&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 Mar 2018 17:30:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754858#M5704</guid>
      <dc:creator>roklipar</dc:creator>
      <dc:date>2018-03-31T17:30:03Z</dc:date>
    </item>
    <item>
      <title>Re: I2C range extender PCA9507</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754859#M5705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;What's your meaning 'I have PCA9507 on both side '?&lt;/P&gt;&lt;P&gt;It can drive a load up to 1400 pF or distance of 18 m on port A, and 400 pF on port B. Capacitive load decide the distance.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 06:00:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754859#M5705</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2018-04-04T06:00:25Z</dc:date>
    </item>
    <item>
      <title>Re: I2C range extender PCA9507</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754860#M5706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Meaning that PCA9507 is on master and slave side, facing, with port A, towards cable or each other.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can understand that 1400pF is the limit which then defines the actual lenght of line or cable itself.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;+-----+&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; +-----+&lt;/P&gt;&lt;P&gt;---B port ---|&amp;nbsp; IC&amp;nbsp; |-----A port------cable-----A port-----|&amp;nbsp; IC&amp;nbsp; |----B port-----&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;+-----+&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; +-----+&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 06:12:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754860#M5706</guid>
      <dc:creator>roklipar</dc:creator>
      <dc:date>2018-04-04T06:12:29Z</dc:date>
    </item>
    <item>
      <title>Re: I2C range extender PCA9507</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754861#M5707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What 's your A port to A port distance?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Apr 2018 23:22:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754861#M5707</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2018-04-04T23:22:39Z</dc:date>
    </item>
    <item>
      <title>Re: I2C range extender PCA9507</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754862#M5708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Port A on PCA9507 (pins 2 and 3).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Apr 2018 05:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/754862#M5708</guid>
      <dc:creator>roklipar</dc:creator>
      <dc:date>2018-04-05T05:11:15Z</dc:date>
    </item>
    <item>
      <title>Re: I2C range extender PCA9507</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/1816857#M21401</link>
      <description>&lt;P&gt;I have the same question and I see it was not totally answered here...&lt;/P&gt;&lt;P&gt;Is it better to connect two PCA9507's port-A together or Port-A to B when sending I2C over a 3-foot cable?&lt;/P&gt;&lt;P&gt;My testing shows that Port-A to B seems to be more stable.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 21:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/I2C-range-extender-PCA9507/m-p/1816857#M21401</guid>
      <dc:creator>EricC5</dc:creator>
      <dc:date>2024-02-27T21:53:11Z</dc:date>
    </item>
  </channel>
</rss>