<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem with Speaker in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-Speaker/m-p/151925#M569</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Solution:&lt;/DIV&gt;&lt;DIV&gt;The output audio device can be selected in the registry of the i.MX31 PDK &lt;SPAN class="yshortcuts"&gt;Windows CE&lt;/SPAN&gt; 6.0 BSP. For more information, please refer to the Section 4.4.6.2 "Optional Audio Driver Runtime Configuration Registry Settings" of the "i.MX31 PDK Windows Embedded CE 6.0 Reference Manual" (pdk13_imx31_WinECE60_RefManual.pdf) document, included in the BSP documentation bundle.&lt;/DIV&gt;&lt;DIV&gt;Also, please refer to the PMIC_AUDIO_OUTPUT_PORT enum definition, that can be found in the&lt;/DIV&gt;&lt;DIV&gt;%WINCEROOT%\PLATFORM\COMMON\SRC\SOC\FREESCALE\PMIC\INC\pmic_audio.h file. So, for the [HKEY_LOCAL_MACHINE\Drivers\BuiltIn\Audio\PMIC\Config\Playback] key, please try to use various PMIC_AUDIO_OUTPUT_PORT enum values. In particular, please try to use the value of 0x100 for "LeftChannel" and 0x200 for "RightChannel" instead of current 0x40 and 0x80.&lt;BR /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Feb 2009 19:00:58 GMT</pubDate>
    <dc:creator>Justin85</dc:creator>
    <dc:date>2009-02-13T19:00:58Z</dc:date>
    <item>
      <title>Problem with Speaker</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-Speaker/m-p/151924#M568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Using iMX31 MAX PDK WinCE, with iMX31 WinCE 6.0 SDK. Without any modification on the origin WinCE source code, I'm having problem on enabling speaker.&lt;BR /&gt;For some reason the speaker on board isn't working, but headset is working fine by plugging in to Audio/Video jack.&lt;BR /&gt;&lt;BR /&gt;I don't see any speaker configuration on winCE itself. Is there any settings has to be done or drivers to install to trigger the speaker on?&lt;BR /&gt;Please help.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2009 00:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-Speaker/m-p/151924#M568</guid>
      <dc:creator>Justin85</dc:creator>
      <dc:date>2009-02-12T00:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Speaker</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-Speaker/m-p/151925#M569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Solution:&lt;/DIV&gt;&lt;DIV&gt;The output audio device can be selected in the registry of the i.MX31 PDK &lt;SPAN class="yshortcuts"&gt;Windows CE&lt;/SPAN&gt; 6.0 BSP. For more information, please refer to the Section 4.4.6.2 "Optional Audio Driver Runtime Configuration Registry Settings" of the "i.MX31 PDK Windows Embedded CE 6.0 Reference Manual" (pdk13_imx31_WinECE60_RefManual.pdf) document, included in the BSP documentation bundle.&lt;/DIV&gt;&lt;DIV&gt;Also, please refer to the PMIC_AUDIO_OUTPUT_PORT enum definition, that can be found in the&lt;/DIV&gt;&lt;DIV&gt;%WINCEROOT%\PLATFORM\COMMON\SRC\SOC\FREESCALE\PMIC\INC\pmic_audio.h file. So, for the [HKEY_LOCAL_MACHINE\Drivers\BuiltIn\Audio\PMIC\Config\Playback] key, please try to use various PMIC_AUDIO_OUTPUT_PORT enum values. In particular, please try to use the value of 0x100 for "LeftChannel" and 0x200 for "RightChannel" instead of current 0x40 and 0x80.&lt;BR /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Feb 2009 19:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-Speaker/m-p/151925#M569</guid>
      <dc:creator>Justin85</dc:creator>
      <dc:date>2009-02-13T19:00:58Z</dc:date>
    </item>
  </channel>
</rss>