<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: PCA9539PW Output issue</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9539PW-Output-issue/m-p/735768#M5496</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I assume that you are setting the corresponding pins as outputs and that you are using the registers 2 and 3 for the logic levels (&lt;EM&gt;Note that if some pin is set as input, the bit values in this register has no effect).&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case, please review the image below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/skins/images/8FC228D08C4BE992E2313B528972C5E5/responsive_peak/images/image_not_found.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As we can see, the pin 11 corresponds to the IO0_7 and so on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please verify that you are configuring the correct pin? &lt;STRONG&gt;Could you please share your initialization process? &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jan 2018 20:23:41 GMT</pubDate>
    <dc:creator>david_diaz</dc:creator>
    <dc:date>2018-01-23T20:23:41Z</dc:date>
    <item>
      <title>PCA9539PW Output issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9539PW-Output-issue/m-p/735767#M5495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Currently using the PCA 9539PW IO expander. Now I can communicate with it and tell it to output individual outputs (works perfectly). However problems arise when I wish to write to pins 7 and 11. What actually happens is that Pin 8 and 11 get set instead. Then when I set Pin 8 and 11(just to see what happens), Pin 7, 8 and 11 are all set!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That seems to me like it is erroneous behavior. Like I mentioned before, I can set individual pins, problems arise when I wish to set 2 pins at a time!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jan 2018 13:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9539PW-Output-issue/m-p/735767#M5495</guid>
      <dc:creator>yashveerrampars</dc:creator>
      <dc:date>2018-01-18T13:12:51Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9539PW Output issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9539PW-Output-issue/m-p/735768#M5496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I assume that you are setting the corresponding pins as outputs and that you are using the registers 2 and 3 for the logic levels (&lt;EM&gt;Note that if some pin is set as input, the bit values in this register has no effect).&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case, please review the image below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/skins/images/8FC228D08C4BE992E2313B528972C5E5/responsive_peak/images/image_not_found.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As we can see, the pin 11 corresponds to the IO0_7 and so on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please verify that you are configuring the correct pin? &lt;STRONG&gt;Could you please share your initialization process? &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2018 20:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9539PW-Output-issue/m-p/735768#M5496</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2018-01-23T20:23:41Z</dc:date>
    </item>
  </channel>
</rss>