<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 10W Wireless Charger(TX, Automotive) in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/10W-Wireless-Charger-TX-Automotive/m-p/732125#M5460</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We want to make 10W TX wireless charger(automotive).&lt;/P&gt;&lt;P&gt;But NXP has 15w(mwct101xA) and 5w(mwct100xA). Then 101xA&amp;nbsp;is a proper solution for&amp;nbsp;10W solution?&lt;/P&gt;&lt;P&gt;I guess 15W solution itself can give 10W to RX only if RX requests 10W to TX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I wonder if there is something for reducing BOM,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If yes, what needs to be modified on both hw &amp;amp; sw sides?&lt;/P&gt;&lt;P&gt;For example, WCT-15WTXAuto uses a Digital buck/boost. The Rail voltage&amp;nbsp; is up to 25V approximately.&lt;/P&gt;&lt;P&gt;if a 10W Solution, such a high rail voltage would not be required. So is the digital duck/boost able to be replaced with cheaper one( max 1x Voltage range)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On SW side, there will be some parameters related with voltage or&amp;nbsp; power limit. I wonder i fthese parameter also should be modified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; BR,&lt;/P&gt;&lt;P&gt;Devin&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 May 2018 01:49:17 GMT</pubDate>
    <dc:creator>devinpark</dc:creator>
    <dc:date>2018-05-08T01:49:17Z</dc:date>
    <item>
      <title>10W Wireless Charger(TX, Automotive)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/10W-Wireless-Charger-TX-Automotive/m-p/732125#M5460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We want to make 10W TX wireless charger(automotive).&lt;/P&gt;&lt;P&gt;But NXP has 15w(mwct101xA) and 5w(mwct100xA). Then 101xA&amp;nbsp;is a proper solution for&amp;nbsp;10W solution?&lt;/P&gt;&lt;P&gt;I guess 15W solution itself can give 10W to RX only if RX requests 10W to TX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I wonder if there is something for reducing BOM,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If yes, what needs to be modified on both hw &amp;amp; sw sides?&lt;/P&gt;&lt;P&gt;For example, WCT-15WTXAuto uses a Digital buck/boost. The Rail voltage&amp;nbsp; is up to 25V approximately.&lt;/P&gt;&lt;P&gt;if a 10W Solution, such a high rail voltage would not be required. So is the digital duck/boost able to be replaced with cheaper one( max 1x Voltage range)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On SW side, there will be some parameters related with voltage or&amp;nbsp; power limit. I wonder i fthese parameter also should be modified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; BR,&lt;/P&gt;&lt;P&gt;Devin&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2018 01:49:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/10W-Wireless-Charger-TX-Automotive/m-p/732125#M5460</guid>
      <dc:creator>devinpark</dc:creator>
      <dc:date>2018-05-08T01:49:17Z</dc:date>
    </item>
    <item>
      <title>Re: 10W Wireless Charger(TX, Automotive)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/10W-Wireless-Charger-TX-Automotive/m-p/732126#M5461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Devin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;NXP reference design gives the ability to support 15W RX charging. And it can be used by customers to support 10W output without any change.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;If your customer needs to replace the power input part,&amp;nbsp;he can modify the HW and corresponding SW part accordingly (the source is open).&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;You can contact directly Mr.&amp;nbsp;Dechang Wang for the support.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Best regards,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 May 2018 08:11:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/10W-Wireless-Charger-TX-Automotive/m-p/732126#M5461</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2018-05-10T08:11:37Z</dc:date>
    </item>
  </channel>
</rss>