<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic trying to find the right processor in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/trying-to-find-the-right-processor/m-p/716811#M5302</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to find a processor but I am having trouble interpreting the datasheets. I am looking for a processor that can do the following: that can run 2 cameras at 1080x1920 resolution at 60fps each while running a android OS, WIFI compatible and obviously must have two inputs for the two cameras. Can someone help me find a processor that can do this or who I should ask?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Oct 2017 01:03:45 GMT</pubDate>
    <dc:creator>adamh</dc:creator>
    <dc:date>2017-10-25T01:03:45Z</dc:date>
    <item>
      <title>trying to find the right processor</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/trying-to-find-the-right-processor/m-p/716811#M5302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to find a processor but I am having trouble interpreting the datasheets. I am looking for a processor that can do the following: that can run 2 cameras at 1080x1920 resolution at 60fps each while running a android OS, WIFI compatible and obviously must have two inputs for the two cameras. Can someone help me find a processor that can do this or who I should ask?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Oct 2017 01:03:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/trying-to-find-the-right-processor/m-p/716811#M5302</guid>
      <dc:creator>adamh</dc:creator>
      <dc:date>2017-10-25T01:03:45Z</dc:date>
    </item>
    <item>
      <title>Re: trying to find the right processor</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/trying-to-find-the-right-processor/m-p/716812#M5303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our i.MX6D and i.MX6Q processors supports up to 3 cameras. &lt;BR /&gt;For parallel interface, the maximum speed of the interface is 240MHz. &lt;BR /&gt;There is a formula in Reference Manual:&lt;BR /&gt;F = FH * FW * FPS * BI * DF &lt;BR /&gt;where FH and FW mean frame size, BI is an overhead that typically is 1.35 (35% overhead), DF is data format (number of cycles needed for each pixel).&lt;BR /&gt;For DF=3 (RGB888) you get 504MHz with this formula (1920*1080*1.35*60*3=503884800) which is more than 240MHz limit.&lt;BR /&gt;And even for DF=2 (YUV422) you get 336MHz which is still more than 240MHz.&lt;BR /&gt;Only in case of DF=1 (bayer format) you get 170MHz: 1920*1080*1.35*60=167961600&lt;BR /&gt;Please refer to chapters 9.1.2 "Video input" and 37.1.2.1.1 "Camera Ports" of i.MX 6Dual/6Quad Applications Processor Reference Manual for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Oct 2017 08:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/trying-to-find-the-right-processor/m-p/716812#M5303</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2017-10-30T08:30:57Z</dc:date>
    </item>
  </channel>
</rss>