<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SC16IS752IPW in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752IPW/m-p/713835#M5280</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The two channels share the same FIFO inside the bridge, therefore if you are using both simultaneously it can cause overwrite of the data. Also overrun errors occur if the transmit data rate exceeds the receive FIFO servicing latency that will occur if you are accessing the FIFO with the 2 channels at the same time, but it's hard to tell if that is the reason of your issue. Could you share the configuration you used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Oct 2017 23:35:43 GMT</pubDate>
    <dc:creator>darioarias</dc:creator>
    <dc:date>2017-10-17T23:35:43Z</dc:date>
    <item>
      <title>SC16IS752IPW</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752IPW/m-p/713834#M5279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use SC 16 IS 752 IPW, but if I communicate with 2 channels simultaneously, I lose data.&lt;BR /&gt;Also, an overrun error has occurred.&lt;BR /&gt;What could be the cause?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 02:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752IPW/m-p/713834#M5279</guid>
      <dc:creator>kame</dc:creator>
      <dc:date>2017-09-26T02:57:45Z</dc:date>
    </item>
    <item>
      <title>Re: SC16IS752IPW</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752IPW/m-p/713835#M5280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The two channels share the same FIFO inside the bridge, therefore if you are using both simultaneously it can cause overwrite of the data. Also overrun errors occur if the transmit data rate exceeds the receive FIFO servicing latency that will occur if you are accessing the FIFO with the 2 channels at the same time, but it's hard to tell if that is the reason of your issue. Could you share the configuration you used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Darío&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Oct 2017 23:35:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752IPW/m-p/713835#M5280</guid>
      <dc:creator>darioarias</dc:creator>
      <dc:date>2017-10-17T23:35:43Z</dc:date>
    </item>
  </channel>
</rss>