<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: RTC read write fails when battery inserted</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703417#M5142</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Try with option - ' battery switch-over function is enabled in standard mode;&amp;nbsp;battery low detection function is enabled'&amp;nbsp; .ie:&amp;nbsp;PM[2:0] = 000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There may be chances like VBAT &amp;gt; VDD . In direct switch mode, it will opt VBAT.&amp;nbsp;If both voltages are close enough say 3.3V, there is a chance for it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 May 2018 09:06:01 GMT</pubDate>
    <dc:creator>chrisjoesebasti</dc:creator>
    <dc:date>2018-05-18T09:06:01Z</dc:date>
    <item>
      <title>RTC read write fails when battery inserted</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703413#M5138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;We are using PCF8523 as RTC for our solution. It works fine if the battery is not inserted. When battery is inserted, the set or read is getting failed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using default values for all registers other than control register 3 .&amp;nbsp;&lt;/P&gt;&lt;P&gt;Control register 3 value is 0xA0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We tried with combinations 0xE0 and 0x80 values for Control register 3 to check the configuration issues, but was not working as expected&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It would be nice if some one could give a help immediately.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Aug 2017 12:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703413#M5138</guid>
      <dc:creator>chrisjoesebasti</dc:creator>
      <dc:date>2017-08-21T12:00:37Z</dc:date>
    </item>
    <item>
      <title>Re: RTC read write fails when battery inserted</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703414#M5139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Joe,&lt;/P&gt;&lt;P&gt;I hope all is great with you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the voltage of the battery that you insert?&lt;/P&gt;&lt;P&gt;Are you using the battery switch-over function?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Sep 2017 15:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703414#M5139</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2017-09-05T15:58:44Z</dc:date>
    </item>
    <item>
      <title>Re: RTC read write fails when battery inserted</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703415#M5140</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The voltage of battery seems to be 3.15 to 3.2 V . The nominal voltage of the device is 3.3 V and during power up state it is showing ~3.3 V. Battery switch over function is enabled . Control register 3 value is 0xA0(battery switch-over function is enabled in direct switching mode,battery low detection function is disabled)&amp;nbsp; and reset of the registers are using default values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Sep 2017 04:35:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703415#M5140</guid>
      <dc:creator>chrisjoesebasti</dc:creator>
      <dc:date>2017-09-06T04:35:10Z</dc:date>
    </item>
    <item>
      <title>Re: RTC read write fails when battery inserted</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703416#M5141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marin :&lt;/P&gt;&lt;P&gt;&amp;nbsp; I meet the same issue on my new project now ,Could you please tell how do you solve this issue ? thanks&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2018 07:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703416#M5141</guid>
      <dc:creator>zhongweihe</dc:creator>
      <dc:date>2018-05-18T07:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: RTC read write fails when battery inserted</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703417#M5142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Try with option - ' battery switch-over function is enabled in standard mode;&amp;nbsp;battery low detection function is enabled'&amp;nbsp; .ie:&amp;nbsp;PM[2:0] = 000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There may be chances like VBAT &amp;gt; VDD . In direct switch mode, it will opt VBAT.&amp;nbsp;If both voltages are close enough say 3.3V, there is a chance for it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2018 09:06:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703417#M5142</guid>
      <dc:creator>chrisjoesebasti</dc:creator>
      <dc:date>2018-05-18T09:06:01Z</dc:date>
    </item>
    <item>
      <title>Re: RTC read write fails when battery inserted</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703418#M5143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastin:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks your support ,our PM[2:0]=000 , Vbat=3V ,VDD=3.3V . below is the log which&amp;nbsp; we read from PCF8523 , it means the default value is 2085-07-14? and sometime some PCBAs can't not enter into the system.&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;SPAN style="color: #1f497d; font-size: medium; font-family: Calibri;"&gt;rtc-pcf8523 2-0068: setting system clock to 2085-07-14 01:03:14 UTC (3645910994)&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 May 2018 01:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/RTC-read-write-fails-when-battery-inserted/m-p/703418#M5143</guid>
      <dc:creator>zhongweihe</dc:creator>
      <dc:date>2018-05-21T01:50:53Z</dc:date>
    </item>
  </channel>
</rss>