<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックPF3000 input power</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PF3000-input-power/m-p/694052#M4992</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the SMARC standard for SOM applications. The input power requirements are 3.0V to 5.25V.&lt;/P&gt;&lt;P&gt;Can I use the PF3000 for such input requirements? (I failed to understand the sentence " Input voltage range: 2.8 V to 4.5 V or 3.7 V to 5.5 V")&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Noam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 28 May 2017 09:10:29 GMT</pubDate>
    <dc:creator>noamweidenfeld</dc:creator>
    <dc:date>2017-05-28T09:10:29Z</dc:date>
    <item>
      <title>PF3000 input power</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PF3000-input-power/m-p/694052#M4992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the SMARC standard for SOM applications. The input power requirements are 3.0V to 5.25V.&lt;/P&gt;&lt;P&gt;Can I use the PF3000 for such input requirements? (I failed to understand the sentence " Input voltage range: 2.8 V to 4.5 V or 3.7 V to 5.5 V")&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Noam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 May 2017 09:10:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PF3000-input-power/m-p/694052#M4992</guid>
      <dc:creator>noamweidenfeld</dc:creator>
      <dc:date>2017-05-28T09:10:29Z</dc:date>
    </item>
  </channel>
</rss>