<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックBasic TX / RX communication between KW01s</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Basic-TX-RX-communication-between-KW01s/m-p/693787#M4984</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to establish basic TX and RX communication between MRB-KW019030JA and USB-KW019032.&lt;/P&gt;&lt;P&gt;USB-KW019032 config:&lt;BR /&gt;- RX Mode&lt;BR /&gt;- Configured to RX at 865 Mhz and 4800bps&lt;BR /&gt;- Fixed Packet Length - 5&lt;BR /&gt;- Sync word of 2 bytes - 0x90,4E&lt;BR /&gt;MRB-KW019030JA config:&lt;BR /&gt;- TX Mode (keeps sending 1 packet of 5 byte payload every second)&lt;BR /&gt;- Configured to TX at 865 Mhz and 4800bps&lt;BR /&gt;- Fixed Packet Length - 5&lt;BR /&gt;- Sync word of 2 bytes - 0x90,4E&lt;/P&gt;&lt;P&gt;(Attached spectrum analyzer snapshot of RF transmit @ 865Mhz)&lt;/P&gt;&lt;P&gt;TX is issuing with PacketSent Interrupt, hence seems right.&lt;BR /&gt;RX is responding with RXReady so ready to receive And even sets Rssi bit, but doesn't receive anythign (sync match bit is not setting).&lt;/P&gt;&lt;P&gt;If I lower threshold, RX receives noise and issues Sync match (only if TX board is OFF). If I turn ON the TX board nothing is received.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 May 2017 10:38:09 GMT</pubDate>
    <dc:creator>saurabhjhamb</dc:creator>
    <dc:date>2017-05-26T10:38:09Z</dc:date>
    <item>
      <title>Basic TX / RX communication between KW01s</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Basic-TX-RX-communication-between-KW01s/m-p/693787#M4984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to establish basic TX and RX communication between MRB-KW019030JA and USB-KW019032.&lt;/P&gt;&lt;P&gt;USB-KW019032 config:&lt;BR /&gt;- RX Mode&lt;BR /&gt;- Configured to RX at 865 Mhz and 4800bps&lt;BR /&gt;- Fixed Packet Length - 5&lt;BR /&gt;- Sync word of 2 bytes - 0x90,4E&lt;BR /&gt;MRB-KW019030JA config:&lt;BR /&gt;- TX Mode (keeps sending 1 packet of 5 byte payload every second)&lt;BR /&gt;- Configured to TX at 865 Mhz and 4800bps&lt;BR /&gt;- Fixed Packet Length - 5&lt;BR /&gt;- Sync word of 2 bytes - 0x90,4E&lt;/P&gt;&lt;P&gt;(Attached spectrum analyzer snapshot of RF transmit @ 865Mhz)&lt;/P&gt;&lt;P&gt;TX is issuing with PacketSent Interrupt, hence seems right.&lt;BR /&gt;RX is responding with RXReady so ready to receive And even sets Rssi bit, but doesn't receive anythign (sync match bit is not setting).&lt;/P&gt;&lt;P&gt;If I lower threshold, RX receives noise and issues Sync match (only if TX board is OFF). If I turn ON the TX board nothing is received.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 May 2017 10:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Basic-TX-RX-communication-between-KW01s/m-p/693787#M4984</guid>
      <dc:creator>saurabhjhamb</dc:creator>
      <dc:date>2017-05-26T10:38:09Z</dc:date>
    </item>
  </channel>
</rss>