<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: Problem sending data on CANBUS thorugh UJA113x System Basis Chip (SBC).</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690642#M4940</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dietmar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Earlier the device was booting up to Forced Normal Mode and CAN communication was working perfectly. Later, I programmed the NVM(0x71 to 0x74) and 0x75(CRC) with correct value as the device powers up and goes to standby mode after performing a reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;which device are you programming?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Im Programming UJA1131F5V0 device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Do you have proper supplies on Vbat, did you connect Vcan?&lt;/P&gt;&lt;P&gt;Yes, Vbat is 12.3v, &amp;nbsp;Currently, On my Board VCAN is showing 0 v. I'm assuming that getting out of Forced Normal Mode has caused this transition to happen from 5v to&amp;nbsp;0v or I might have damaged the board while testing :smileysilly:&amp;nbsp;due to which VCAN is showing 0v.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;If you are after inital power up in Forced normal mode CAN Transceiver should be already working.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;No, As I reprogrammed the NVM. Currently FNMC = 0(Forced Normal Mode Disabled) &amp;amp; SDMC = 1(Software Development Mode Enabled). So, On power up It goes to standby mode and then I&amp;nbsp;send command (0x0207) to send it into normal mode(I want to operate the chip in NORMAL Mode in future rather than Forced Normal Mode).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;did you lock MTP after programming reg 70 to 74 with CRC value and did you see reset happen afterwards?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Yes I placed the correct CRC Value in 0x75 register and reset occurred.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Take a look with the scope if you see your CAN H , CAN L pin moving&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;CANH and CANL both are at 2.524 Volts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a Question to ask:&lt;/P&gt;&lt;P&gt;- PIN NO. 20 on SBC (VCAN), does it generate a 5v o/p or should it be given a 5v i/p ???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Abhishek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Aug 2017 13:07:37 GMT</pubDate>
    <dc:creator>abhi1992</dc:creator>
    <dc:date>2017-08-03T13:07:37Z</dc:date>
    <item>
      <title>Problem sending data on CANBUS thorugh UJA113x System Basis Chip (SBC).</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690640#M4938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am facing an issue while using &lt;STRONG&gt;UJA113x System Basis Chip (SBC)&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;See Link:&amp;nbsp;&lt;A class="link-titled" href="http://www.nxp.com/docs/en/data-sheet/UJA113X_SER.pdf" title="http://www.nxp.com/docs/en/data-sheet/UJA113X_SER.pdf"&gt;http://www.nxp.com/docs/en/data-sheet/UJA113X_SER.pdf&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have programmed the NVM (0x71 to 0x74) to get out of Forced Normal Mode. by setting&amp;nbsp;FNMC = 0 and SDMC = 1.&lt;/P&gt;&lt;P&gt;On-Startup I send the following SPI commands to device:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CMD 1: &amp;nbsp;(0x0207) - Write operation at MC(Mode Control) 0x01h register, to send the device into normal mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CMD 2: &amp;nbsp;(0x4002) -&amp;nbsp;&lt;SPAN&gt;Write operation at CAN Control register 0x20h, to disable CAN transceiver&amp;nbsp;shutdown(CSC bits) and select operating mode(CMC bits) to Active Mode(under voltage&amp;nbsp;disabled).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have made sure that data is available on TXDC pin . But still, I m not able to see data on CANBUS i.e. CANH and CANL (pin 21 and pin 22). I tried to see data on CANBUS through logic analyser but both both lines are at LOW level.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Are there any more registers which need to be configured ?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2017 07:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690640#M4938</guid>
      <dc:creator>abhi1992</dc:creator>
      <dc:date>2017-08-02T07:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: Problem sending data on CANBUS thorugh UJA113x System Basis Chip (SBC).</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690641#M4939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which device are you programming?&lt;/P&gt;&lt;P&gt;Do you have proper supplies on Vbat, did you connect Vcan?&lt;/P&gt;&lt;P&gt;If you are after inital power up in Forced normal mode CAN Transceiver should be already working.&lt;/P&gt;&lt;P&gt;did you lock MTP after programming reg 70 to 74 with CRC value and did you see reset happen afterwards?&lt;/P&gt;&lt;P&gt;Take a look with the scope if you see your CAN H , CAN L pin moving&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Aug 2017 16:58:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690641#M4939</guid>
      <dc:creator>dietmarschmid</dc:creator>
      <dc:date>2017-08-02T16:58:59Z</dc:date>
    </item>
    <item>
      <title>Re: Problem sending data on CANBUS thorugh UJA113x System Basis Chip (SBC).</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690642#M4940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dietmar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Earlier the device was booting up to Forced Normal Mode and CAN communication was working perfectly. Later, I programmed the NVM(0x71 to 0x74) and 0x75(CRC) with correct value as the device powers up and goes to standby mode after performing a reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;which device are you programming?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Im Programming UJA1131F5V0 device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;Do you have proper supplies on Vbat, did you connect Vcan?&lt;/P&gt;&lt;P&gt;Yes, Vbat is 12.3v, &amp;nbsp;Currently, On my Board VCAN is showing 0 v. I'm assuming that getting out of Forced Normal Mode has caused this transition to happen from 5v to&amp;nbsp;0v or I might have damaged the board while testing :smileysilly:&amp;nbsp;due to which VCAN is showing 0v.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;If you are after inital power up in Forced normal mode CAN Transceiver should be already working.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;No, As I reprogrammed the NVM. Currently FNMC = 0(Forced Normal Mode Disabled) &amp;amp; SDMC = 1(Software Development Mode Enabled). So, On power up It goes to standby mode and then I&amp;nbsp;send command (0x0207) to send it into normal mode(I want to operate the chip in NORMAL Mode in future rather than Forced Normal Mode).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;did you lock MTP after programming reg 70 to 74 with CRC value and did you see reset happen afterwards?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Yes I placed the correct CRC Value in 0x75 register and reset occurred.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Take a look with the scope if you see your CAN H , CAN L pin moving&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;CANH and CANL both are at 2.524 Volts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a Question to ask:&lt;/P&gt;&lt;P&gt;- PIN NO. 20 on SBC (VCAN), does it generate a 5v o/p or should it be given a 5v i/p ???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Abhishek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 13:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690642#M4940</guid>
      <dc:creator>abhi1992</dc:creator>
      <dc:date>2017-08-03T13:07:37Z</dc:date>
    </item>
    <item>
      <title>Re: Problem sending data on CANBUS thorugh UJA113x System Basis Chip (SBC).</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690643#M4941</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Dietmar,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, I had one more doubt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have enabled the SDMC bit (SDMC = 1) in 0x74 register of NVM. i.e. Software development mode is enabled&lt;/P&gt;&lt;P&gt;In datasheet page no. 20 they(*manufacturers) have mentioned it as " &lt;EM&gt;Software Development mode (Software Development mode is provided&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;for test purposes and is not an SBC operating mode&lt;/EM&gt; " can it be a possible reason for VCAN to be 0v?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Abhishek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 13:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690643#M4941</guid>
      <dc:creator>abhi1992</dc:creator>
      <dc:date>2017-08-03T13:31:35Z</dc:date>
    </item>
    <item>
      <title>Re: Problem sending data on CANBUS thorugh UJA113x System Basis Chip (SBC).</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690644#M4942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Abishek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vcan is an input, &amp;nbsp;needs concection&amp;nbsp;to a 5V &amp;nbsp;for example V1 or V2. &amp;nbsp;&lt;/P&gt;&lt;P&gt;did you leave it open?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 13:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690644#M4942</guid>
      <dc:creator>dietmarschmid</dc:creator>
      <dc:date>2017-08-03T13:53:30Z</dc:date>
    </item>
    <item>
      <title>Re: Problem sending data on CANBUS thorugh UJA113x System Basis Chip (SBC).</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690645#M4943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dietmar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your support. It helped a lot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On My board pin no. (2&amp;amp;3) i.e V2 and VEXT are shorted and are connected to VCAN. The output from V2 is connected to VCAN and I noticed that V2C bits(3&amp;amp; 2) were set to '00' in Regulator Control register (0x10h). So, I reprogrammed it '10' and now VCAN is getting 5v . CAN communication is working fine now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Abhishek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 10:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690645#M4943</guid>
      <dc:creator>abhi1992</dc:creator>
      <dc:date>2017-08-04T10:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: Problem sending data on CANBUS thorugh UJA113x System Basis Chip (SBC).</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690646#M4944</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dietmar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm facing a problem in restoring factory preset values. As mentioned in datasheet, pg no - 88&amp;nbsp; &lt;STRONG&gt;&lt;EM&gt;'7.13.2 Restoring factory preset values'&lt;/EM&gt;&lt;/STRONG&gt;. I applied the mentioned changes as follows: &lt;/P&gt;&lt;P&gt;1. Reset pin directly connected to GND.&lt;/P&gt;&lt;P&gt;2. CANH is pulled up to VBAT(12V in my case), with a 33K (1/4 W) resistor.&lt;/P&gt;&lt;P&gt;3. CANL is pulled down to GND, with a 33K (1/4 W) resistor.&lt;/P&gt;&lt;P&gt;After applying this configuration I switch ON the power supply for 5 secs and then turn it OFF. After this when I turn ON the supply it again enters into Stand-By Mode rather than Forced Normal Mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if you have tried to restore factory preset values and what configuration you applied.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Abhishek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Sep 2017 13:31:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-sending-data-on-CANBUS-thorugh-UJA113x-System-Basis-Chip/m-p/690646#M4944</guid>
      <dc:creator>abhi1992</dc:creator>
      <dc:date>2017-09-05T13:31:38Z</dc:date>
    </item>
  </channel>
</rss>