<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SJA1000 bus errors in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1000-bus-errors/m-p/681641#M4828</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the SJA1000T in a circuit, with a PIC processor and TI transceiver. I have put it into local self test mode, writing 0x10 into CDR when the buffer is loaded. I get an initial transmission, but with a start frame error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything wrong with the circuit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried different configurations of the output FETs (OCP0, OCN0 and OCPOL0) with no effect and no transmission.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Initialisation:&lt;/P&gt;&lt;P&gt;Intel mode,&lt;/P&gt;&lt;P&gt;reset mode,&lt;/P&gt;&lt;P&gt;CDR = CLKOUT=off, PeliCAN mode, bypass comparator&lt;/P&gt;&lt;P&gt;OCR = various different options&lt;/P&gt;&lt;P&gt;speed = 1Mbps (16MHz sys clock, btr0=0x00, btr1=0x14)&lt;/P&gt;&lt;P&gt;set all AMR to 0xff (disabled, I believe)&lt;/P&gt;&lt;P&gt;IER = 0xff (enable all interrupts) -&amp;gt; don't see any on the processor&lt;/P&gt;&lt;P&gt;set mode to local-self test (bit 2 set)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For transmission:&lt;/P&gt;&lt;P&gt;write the ID, write INFO and then data&lt;/P&gt;&lt;P&gt;Set bit 4 in CMR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I doing anything wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Jun 2017 13:11:54 GMT</pubDate>
    <dc:creator>iankey</dc:creator>
    <dc:date>2017-06-09T13:11:54Z</dc:date>
    <item>
      <title>SJA1000 bus errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1000-bus-errors/m-p/681641#M4828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the SJA1000T in a circuit, with a PIC processor and TI transceiver. I have put it into local self test mode, writing 0x10 into CDR when the buffer is loaded. I get an initial transmission, but with a start frame error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything wrong with the circuit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried different configurations of the output FETs (OCP0, OCN0 and OCPOL0) with no effect and no transmission.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Initialisation:&lt;/P&gt;&lt;P&gt;Intel mode,&lt;/P&gt;&lt;P&gt;reset mode,&lt;/P&gt;&lt;P&gt;CDR = CLKOUT=off, PeliCAN mode, bypass comparator&lt;/P&gt;&lt;P&gt;OCR = various different options&lt;/P&gt;&lt;P&gt;speed = 1Mbps (16MHz sys clock, btr0=0x00, btr1=0x14)&lt;/P&gt;&lt;P&gt;set all AMR to 0xff (disabled, I believe)&lt;/P&gt;&lt;P&gt;IER = 0xff (enable all interrupts) -&amp;gt; don't see any on the processor&lt;/P&gt;&lt;P&gt;set mode to local-self test (bit 2 set)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For transmission:&lt;/P&gt;&lt;P&gt;write the ID, write INFO and then data&lt;/P&gt;&lt;P&gt;Set bit 4 in CMR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I doing anything wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2017 13:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1000-bus-errors/m-p/681641#M4828</guid>
      <dc:creator>iankey</dc:creator>
      <dc:date>2017-06-09T13:11:54Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1000 bus errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1000-bus-errors/m-p/681642#M4829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I contacted my colleague and I am waiting for his answer. I will write you back as soon as I get any feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jun 2017 08:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1000-bus-errors/m-p/681642#M4829</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-06-19T08:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1000 bus errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1000-bus-errors/m-p/681643#M4830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I received answer from my colleague:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;There is no problem in the device.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Does customer use AN97067 App note?&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;I don’t see Acceptance code register set, cleared? Is that done?&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;CMR bit 4 is go to sleep?&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24732i30FF3A187FDB2C84/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;Timings can also be wrong...&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 07:07:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1000-bus-errors/m-p/681643#M4830</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-06-20T07:07:27Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1000 bus errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1000-bus-errors/m-p/681644#M4831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the information. Yes, I am using the app note AN97076 as well as the data sheet. I didn't realise there was a contention in the data. Following section 5.7 of the app note, is states "Self Reception Request is CMR=0x10". In fact, I have datasheet 2000 Jan 04 and it states on page 23, CMR.4 = SRR (Self Reception Request". When was this bit altered and where can I find the 'correct' datasheet?&amp;nbsp; If CMR.4 is now go to sleep, how do loopback/self-tests get performed?&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;Ian&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;(PS. Apologies for the delay in responding, I was out of the country for a week&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 10:36:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1000-bus-errors/m-p/681644#M4831</guid>
      <dc:creator>iankey</dc:creator>
      <dc:date>2017-06-26T10:36:52Z</dc:date>
    </item>
  </channel>
</rss>