<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SC16IS750 interrupt in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS750-interrupt/m-p/675318#M4754</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to use&amp;nbsp;SC16IS750 to bridge I2C to UART. Therefore I would like to use IRQ functionality to prevent software from the requirement to poll for status. For the physical connection in datasheet is mentioned, to use 1k pull-up for 3V3 or 1k5 for 2V5 supply. Would it be possible to use 100k connected to 1V8 power supply as well? &amp;nbsp;The point is, that I have some host device which hs&amp;nbsp;just 1V8 compatible pins and I'd like to prevent some additional level shifters.&lt;/P&gt;&lt;P&gt;I'm just wondering about pull-up resistor value requirement as based on datasheet, IRQ pin is able to sink up to 4mA, why does pull-up resistor for 2V5 be higher than connected to 3V3?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 May 2017 13:17:19 GMT</pubDate>
    <dc:creator>robertkaliauer</dc:creator>
    <dc:date>2017-05-10T13:17:19Z</dc:date>
    <item>
      <title>SC16IS750 interrupt</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS750-interrupt/m-p/675318#M4754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to use&amp;nbsp;SC16IS750 to bridge I2C to UART. Therefore I would like to use IRQ functionality to prevent software from the requirement to poll for status. For the physical connection in datasheet is mentioned, to use 1k pull-up for 3V3 or 1k5 for 2V5 supply. Would it be possible to use 100k connected to 1V8 power supply as well? &amp;nbsp;The point is, that I have some host device which hs&amp;nbsp;just 1V8 compatible pins and I'd like to prevent some additional level shifters.&lt;/P&gt;&lt;P&gt;I'm just wondering about pull-up resistor value requirement as based on datasheet, IRQ pin is able to sink up to 4mA, why does pull-up resistor for 2V5 be higher than connected to 3V3?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 May 2017 13:17:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS750-interrupt/m-p/675318#M4754</guid>
      <dc:creator>robertkaliauer</dc:creator>
      <dc:date>2017-05-10T13:17:19Z</dc:date>
    </item>
    <item>
      <title>Re: SC16IS750 interrupt</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS750-interrupt/m-p/675319#M4755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No infos?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 13:07:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS750-interrupt/m-p/675319#M4755</guid>
      <dc:creator>robertkaliauer</dc:creator>
      <dc:date>2017-05-15T13:07:47Z</dc:date>
    </item>
  </channel>
</rss>