<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: SC16IS752IPW Reset</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752IPW-Reset/m-p/627641#M4196</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael Pfab,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I do believe that the cause of the reset you are seen is the ripple you are seen at the Reset input.&lt;/P&gt;&lt;P&gt;Suggest you to add a decoupling capacitor on this rail to try to reduce the ripple.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Nov 2016 16:59:42 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2016-11-30T16:59:42Z</dc:date>
    <item>
      <title>SC16IS752IPW Reset</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752IPW-Reset/m-p/627640#M4195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello together,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the SC16IS752IPW 16 times on a big PCB.&lt;/P&gt;&lt;P&gt;Since I made a new revision of the PCB the SC16IS752IPW allways looses its setting (makes a reset) after switching a relais near the chip. The astonishing thing is, that between the revision bevor and the actual one I din't change anything around the Relais or the&amp;nbsp; SC16IS752IPW.&lt;/P&gt;&lt;P&gt;Measuring the souroundings of the chip I get a ripple at the 3.3V supply voltage (400mVpp for 1us) at the Reset input (1Vpp for 100ns) and at the I²S Data/Clock (1Vpp for 100ns) while switching the Reliais. Can this be the reason for the reset of the chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Michael Pfab&lt;/P&gt;&lt;H1&gt;&lt;/H1&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 11:00:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752IPW-Reset/m-p/627640#M4195</guid>
      <dc:creator>Pudl</dc:creator>
      <dc:date>2016-11-28T11:00:12Z</dc:date>
    </item>
    <item>
      <title>Re: SC16IS752IPW Reset</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752IPW-Reset/m-p/627641#M4196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael Pfab,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I do believe that the cause of the reset you are seen is the ripple you are seen at the Reset input.&lt;/P&gt;&lt;P&gt;Suggest you to add a decoupling capacitor on this rail to try to reduce the ripple.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Nov 2016 16:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS752IPW-Reset/m-p/627641#M4196</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2016-11-30T16:59:42Z</dc:date>
    </item>
  </channel>
</rss>