<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Where is Oscillator Stop (OS) status bit in PCF85263A RTC registers? in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Where-is-Oscillator-Stop-OS-status-bit-in-PCF85263A-RTC/m-p/625222#M4159</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bob,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is a bit confusing, but the OS bit is bit 7 in the Seconds Register (01h):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Seconds reg.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9634iB02274701A1ACD1A/image-size/large?v=v2&amp;amp;px=999" role="button" title="Seconds reg.jpg" alt="Seconds reg.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Nov 2016 19:44:10 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2016-11-29T19:44:10Z</dc:date>
    <item>
      <title>Where is Oscillator Stop (OS) status bit in PCF85263A RTC registers?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Where-is-Oscillator-Stop-OS-status-bit-in-PCF85263A-RTC/m-p/625221#M4158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where is the Oscillator Stop (OS) status bit in PCF85263A RealTimeClock?&amp;nbsp; The Data Sheet talks at length about the bit, but I cannot find it in the control registers.&amp;nbsp; Access to bit is critical to insure the oscillator has not been interrupted&amp;nbsp; - even for a moment.&amp;nbsp; My design uses super capacitor for backup (and internal switch), but backup voltage can go too low for oscillator to keep functioning.&amp;nbsp; Attached are two relevant pages of data sheet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Nov 2016 23:35:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Where-is-Oscillator-Stop-OS-status-bit-in-PCF85263A-RTC/m-p/625221#M4158</guid>
      <dc:creator>bobschilken</dc:creator>
      <dc:date>2016-11-26T23:35:30Z</dc:date>
    </item>
    <item>
      <title>Re: Where is Oscillator Stop (OS) status bit in PCF85263A RTC registers?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Where-is-Oscillator-Stop-OS-status-bit-in-PCF85263A-RTC/m-p/625222#M4159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bob,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is a bit confusing, but the OS bit is bit 7 in the Seconds Register (01h):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Seconds reg.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9634iB02274701A1ACD1A/image-size/large?v=v2&amp;amp;px=999" role="button" title="Seconds reg.jpg" alt="Seconds reg.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2016 19:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Where-is-Oscillator-Stop-OS-status-bit-in-PCF85263A-RTC/m-p/625222#M4159</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2016-11-29T19:44:10Z</dc:date>
    </item>
    <item>
      <title>Re: Where is Oscillator Stop (OS) status bit in PCF85263A RTC registers?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Where-is-Oscillator-Stop-OS-status-bit-in-PCF85263A-RTC/m-p/625223#M4160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you!&amp;nbsp; Appreciate the quick response.&amp;nbsp; Maybe you can recommend adding the bolded words to the text right above Figure 9 in the data sheet.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"The status bit remains set until cleared by &lt;STRONG&gt;writing a 0 to bit 7 of register 0x01&lt;/STRONG&gt; &lt;EM&gt;command&lt;/EM&gt; (see Figure 9). If the bit cannot be cleared, then the oscillator is not running. This method can be used to monitor the&lt;BR /&gt;oscillator and to determine if the supply voltage has reduced to the point where oscillation&lt;BR /&gt;fails."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The rest of the data sheet is very well written.&amp;nbsp; My compliments!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2016 20:25:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Where-is-Oscillator-Stop-OS-status-bit-in-PCF85263A-RTC/m-p/625223#M4160</guid>
      <dc:creator>bobschilken</dc:creator>
      <dc:date>2016-11-29T20:25:26Z</dc:date>
    </item>
  </channel>
</rss>