<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: TJA1145 - Wakeup not happening as expected</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1145-Wakeup-not-happening-as-expected/m-p/609866#M4004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this could be caused by Autonomous CAN biasing. The device only terminates its CAN bus pins to GND while&lt;/P&gt;&lt;P&gt;- the CAN block is in a low-power mode and&lt;/P&gt;&lt;P&gt;- the bus is idle for longer than approximately one second.&lt;/P&gt;&lt;P&gt;Otherwise the CAN bus pins bias towards 2,5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each time there is traffic on the bus (see Fig 9) an internal timer is reset and the bus pins bias towards 2,5V. At bus silence the timer starts counting until about one second. After this silence time the bus biasing changes towards 0V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17646iBD73A82D8D4576E6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So the first frame is not probably received without error due to GND biasing and also makes bus biasing to 2.5V again.&lt;/P&gt;&lt;P&gt;Then if second frame is received within about one second, the transceiver wakeup normally.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See TR1309 Application Hints - High speed CAN transceiver for partial networking TJA1145 (&lt;A href="http://www.nxp.com/documents/report/AH1309_v1_1_Application_Hints_TJA1145.pdf"&gt;http://www.nxp.com/documents/report/AH1309_v1_1_Application_Hints_TJA1145.pdf&lt;/A&gt;) for mor info about this transceiver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Mar 2017 12:21:53 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2017-03-24T12:21:53Z</dc:date>
    <item>
      <title>TJA1145 - Wakeup not happening as expected</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1145-Wakeup-not-happening-as-expected/m-p/609865#M4003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using TJA1145 High-speed CAN transceiver for partial networking. The selective wakeup is configured. But it is observed that the transceiver wakeup do not happen with first frame. But on receiving the second frame the wakeup is successful. &amp;nbsp;Also if there is a significant delay between the first and second&amp;nbsp;frame (two frames must be received within 1sec)&amp;nbsp;also the&amp;nbsp;transceiver do not wakeup. Could you please help us in this regard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 12:24:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1145-Wakeup-not-happening-as-expected/m-p/609865#M4003</guid>
      <dc:creator>maitreya_jain</dc:creator>
      <dc:date>2017-03-22T12:24:39Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1145 - Wakeup not happening as expected</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1145-Wakeup-not-happening-as-expected/m-p/609866#M4004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this could be caused by Autonomous CAN biasing. The device only terminates its CAN bus pins to GND while&lt;/P&gt;&lt;P&gt;- the CAN block is in a low-power mode and&lt;/P&gt;&lt;P&gt;- the bus is idle for longer than approximately one second.&lt;/P&gt;&lt;P&gt;Otherwise the CAN bus pins bias towards 2,5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each time there is traffic on the bus (see Fig 9) an internal timer is reset and the bus pins bias towards 2,5V. At bus silence the timer starts counting until about one second. After this silence time the bus biasing changes towards 0V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17646iBD73A82D8D4576E6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So the first frame is not probably received without error due to GND biasing and also makes bus biasing to 2.5V again.&lt;/P&gt;&lt;P&gt;Then if second frame is received within about one second, the transceiver wakeup normally.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See TR1309 Application Hints - High speed CAN transceiver for partial networking TJA1145 (&lt;A href="http://www.nxp.com/documents/report/AH1309_v1_1_Application_Hints_TJA1145.pdf"&gt;http://www.nxp.com/documents/report/AH1309_v1_1_Application_Hints_TJA1145.pdf&lt;/A&gt;) for mor info about this transceiver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2017 12:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1145-Wakeup-not-happening-as-expected/m-p/609866#M4004</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2017-03-24T12:21:53Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1145 - Wakeup not happening as expected</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1145-Wakeup-not-happening-as-expected/m-p/1502511#M14890</link>
      <description />
      <pubDate>Mon, 08 Aug 2022 09:55:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1145-Wakeup-not-happening-as-expected/m-p/1502511#M14890</guid>
      <dc:creator>chenhuang</dc:creator>
      <dc:date>2022-08-08T09:55:02Z</dc:date>
    </item>
  </channel>
</rss>