<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックPCF8576 question</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCF8576-question/m-p/608746#M3997</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, has the silicon changed in the PCF8576 LCD driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We&amp;nbsp;use two versions (&amp;gt;2k pieces&amp;nbsp;p.a.): a) PCF8576CT and b) PCF8576T (datasheets attached).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Monitoring the 'CLK' pin (pin 4), the PCF8567CT runs at about 200kHz and the backplane signals run at ~68Hz&amp;nbsp;which agrees with the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, the PCF8576T runs at ~600kHz with the backplanes running at 225Hz&amp;nbsp;i.e. ~3x the stated frequency!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By changing the value of a resistor connected between the&amp;nbsp;'OSC' pin&amp;nbsp;(pin 6) and GND, the clock frequency of the PCF8576T can be altered over a wide range&amp;nbsp;to bring it down to the 200kHz specified in the datasheet and beyond.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, changing the resistor value, even up to 500k&amp;nbsp;on the PCF8576CT&amp;nbsp;has no affect on&amp;nbsp;the clock frequency??!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PFC8576CT's frequency, although it is more in tune with the datasheet does however produce a flickering display&amp;nbsp;while the 600kHz PCF8567T does not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has one version become obsolete, if so which? If not, do you intend to continue to produce two wildly different versions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regards, Ron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Dec 2016 17:25:38 GMT</pubDate>
    <dc:creator>ronjoyce</dc:creator>
    <dc:date>2016-12-13T17:25:38Z</dc:date>
    <item>
      <title>PCF8576 question</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF8576-question/m-p/608746#M3997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, has the silicon changed in the PCF8576 LCD driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We&amp;nbsp;use two versions (&amp;gt;2k pieces&amp;nbsp;p.a.): a) PCF8576CT and b) PCF8576T (datasheets attached).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Monitoring the 'CLK' pin (pin 4), the PCF8567CT runs at about 200kHz and the backplane signals run at ~68Hz&amp;nbsp;which agrees with the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, the PCF8576T runs at ~600kHz with the backplanes running at 225Hz&amp;nbsp;i.e. ~3x the stated frequency!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By changing the value of a resistor connected between the&amp;nbsp;'OSC' pin&amp;nbsp;(pin 6) and GND, the clock frequency of the PCF8576T can be altered over a wide range&amp;nbsp;to bring it down to the 200kHz specified in the datasheet and beyond.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, changing the resistor value, even up to 500k&amp;nbsp;on the PCF8576CT&amp;nbsp;has no affect on&amp;nbsp;the clock frequency??!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PFC8576CT's frequency, although it is more in tune with the datasheet does however produce a flickering display&amp;nbsp;while the 600kHz PCF8567T does not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has one version become obsolete, if so which? If not, do you intend to continue to produce two wildly different versions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regards, Ron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 17:25:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF8576-question/m-p/608746#M3997</guid>
      <dc:creator>ronjoyce</dc:creator>
      <dc:date>2016-12-13T17:25:38Z</dc:date>
    </item>
  </channel>
</rss>