<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: ESD protection diode PUSB3F96</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/ESD-protection-diode-PUSB3F96/m-p/597137#M3888</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Both parameters are correct. As you can see in the datasheet it is not a normal "Zener diode", it is a structure with a very specific snap-back feature. Please take a look at Figure 13 of the datasheet (V-I function) and description on the same page, it explains functionality of the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Sep 2016 12:28:48 GMT</pubDate>
    <dc:creator>Bulat</dc:creator>
    <dc:date>2016-09-13T12:28:48Z</dc:date>
    <item>
      <title>ESD protection diode PUSB3F96</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ESD-protection-diode-PUSB3F96/m-p/597136#M3887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems there is a mismatch in the datasheet of PUSB3F96. The breakdown voltage is given with min. 6V and the clamping voltage for positive transients is given with typ. &lt;A href="mailto:4.6V@5.2A"&gt;4.6V@5.2A&lt;/A&gt;. Which one of these two values is correct? Or do I understand something wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 09:08:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ESD-protection-diode-PUSB3F96/m-p/597136#M3887</guid>
      <dc:creator>manfredmoeschl</dc:creator>
      <dc:date>2016-09-07T09:08:59Z</dc:date>
    </item>
    <item>
      <title>Re: ESD protection diode PUSB3F96</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ESD-protection-diode-PUSB3F96/m-p/597137#M3888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Both parameters are correct. As you can see in the datasheet it is not a normal "Zener diode", it is a structure with a very specific snap-back feature. Please take a look at Figure 13 of the datasheet (V-I function) and description on the same page, it explains functionality of the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2016 12:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ESD-protection-diode-PUSB3F96/m-p/597137#M3888</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2016-09-13T12:28:48Z</dc:date>
    </item>
  </channel>
</rss>