<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 SC18IM700 RX and TX pins - TTL or not?</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IM700-RX-and-TX-pins-TTL-or-not/m-p/569681#M3769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am thinking about using the SC18IM700 for RS-232 to I2C conversion. My question is about the RX and TX pins on this chip. Are these real RS-232 signals that go from -5V to +5V or are they TTL serial signals that only go from 0V to +5V? I could not find any information about this on the data sheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if they do go from -5V to +5V, are these values generated internally from the 2.3V-3.6V power supply used to operate the chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Aug 2016 16:54:42 GMT</pubDate>
    <dc:creator>zackjohnson</dc:creator>
    <dc:date>2016-08-04T16:54:42Z</dc:date>
    <item>
      <title>SC18IM700 RX and TX pins - TTL or not?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IM700-RX-and-TX-pins-TTL-or-not/m-p/569681#M3769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am thinking about using the SC18IM700 for RS-232 to I2C conversion. My question is about the RX and TX pins on this chip. Are these real RS-232 signals that go from -5V to +5V or are they TTL serial signals that only go from 0V to +5V? I could not find any information about this on the data sheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if they do go from -5V to +5V, are these values generated internally from the 2.3V-3.6V power supply used to operate the chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Aug 2016 16:54:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IM700-RX-and-TX-pins-TTL-or-not/m-p/569681#M3769</guid>
      <dc:creator>zackjohnson</dc:creator>
      <dc:date>2016-08-04T16:54:42Z</dc:date>
    </item>
    <item>
      <title>Re: SC18IM700 RX and TX pins - TTL or not?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IM700-RX-and-TX-pins-TTL-or-not/m-p/569682#M3770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jack,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The signal levels of the TX and RX pins are as stated on Table 11 in the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to use this device for RS-232 communication over a wire, then you will need an RS-232 line transceiver also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM style="font-weight: normal; font-style: italic; font-size: 11px; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f; text-align: left; text-indent: 0px;"&gt;PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Aug 2016 08:40:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IM700-RX-and-TX-pins-TTL-or-not/m-p/569682#M3770</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2016-08-05T08:40:21Z</dc:date>
    </item>
  </channel>
</rss>