<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Cascading 74LVC595A shift registers in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Cascading-74LVC595A-shift-registers/m-p/554817#M3715</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey, &lt;BR /&gt;the 74LVC595A shift registers reads the incoming data with the rising clock edge. The serial data output is also clocked on the rising edge of the SHCP. Could there be a problem when cascading several 74LVC595A devices, due to propagation delay and&amp;nbsp; hold time? I mean the cascaded register has a hold time of minimum 1.5ns at 3.3V, the data output could have a propagation delay of 1.5ns. This means the second register can see a changing input pin 1.5ns after the clock pulse, so layout effects of a few ps can make my device unfunctional by reading strange things.&lt;/P&gt;&lt;P&gt;Is there a good way to avoid problems like this? Why isn't a additional Q7S flip flop in the device, which latches the data out at the falling clock edge?&lt;/P&gt;&lt;P&gt;Yours Franz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Aug 2016 09:10:50 GMT</pubDate>
    <dc:creator>franzforstmayr</dc:creator>
    <dc:date>2016-08-01T09:10:50Z</dc:date>
    <item>
      <title>Cascading 74LVC595A shift registers</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Cascading-74LVC595A-shift-registers/m-p/554817#M3715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey, &lt;BR /&gt;the 74LVC595A shift registers reads the incoming data with the rising clock edge. The serial data output is also clocked on the rising edge of the SHCP. Could there be a problem when cascading several 74LVC595A devices, due to propagation delay and&amp;nbsp; hold time? I mean the cascaded register has a hold time of minimum 1.5ns at 3.3V, the data output could have a propagation delay of 1.5ns. This means the second register can see a changing input pin 1.5ns after the clock pulse, so layout effects of a few ps can make my device unfunctional by reading strange things.&lt;/P&gt;&lt;P&gt;Is there a good way to avoid problems like this? Why isn't a additional Q7S flip flop in the device, which latches the data out at the falling clock edge?&lt;/P&gt;&lt;P&gt;Yours Franz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2016 09:10:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Cascading-74LVC595A-shift-registers/m-p/554817#M3715</guid>
      <dc:creator>franzforstmayr</dc:creator>
      <dc:date>2016-08-01T09:10:50Z</dc:date>
    </item>
    <item>
      <title>Re: Cascading 74LVC595A shift registers</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Cascading-74LVC595A-shift-registers/m-p/554818#M3716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="caseEventBody"&gt;&lt;SPAN class="caseEventRow"&gt;&lt;SPAN class="cxfeeditemtext feeditemtext"&gt;It should not be a problem, everything will work correctly as you expect.&lt;BR /&gt;If you are going to work at very high clock frequencies, there is a reason to pay attention to clock routing. Specifically, clock delay from the clock source to clock inputs of all shift registers should be the same.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="caseEventBody"&gt;&lt;SPAN class="caseEventRow"&gt;&lt;SPAN class="cxfeeditemtext feeditemtext"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="caseEventBody"&gt;&lt;SPAN class="caseEventRow"&gt;&lt;SPAN class="cxfeeditemtext feeditemtext"&gt;Regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="caseEventBody"&gt;&lt;SPAN class="caseEventRow"&gt;&lt;SPAN class="cxfeeditemtext feeditemtext"&gt;Bulat&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="caseEventBody"&gt;&lt;SPAN class="caseEventRow"&gt;&lt;SPAN class="cxfeeditemtext feeditemtext"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Aug 2016 12:16:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Cascading-74LVC595A-shift-registers/m-p/554818#M3716</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2016-08-03T12:16:24Z</dc:date>
    </item>
  </channel>
</rss>