<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: Problem in generating IF(KHz) using SA612A mixer</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-in-generating-IF-KHz-using-SA612A-mixer/m-p/549952#M3692</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please create a Service request.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/381898"&gt;How I could create a Service Request?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please provide in Service request your schematics, Input and Output traces.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Aug 2016 05:52:09 GMT</pubDate>
    <dc:creator>andrei_skok</dc:creator>
    <dc:date>2016-08-10T05:52:09Z</dc:date>
    <item>
      <title>Problem in generating IF(KHz) using SA612A mixer</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-in-generating-IF-KHz-using-SA612A-mixer/m-p/549951#M3691</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi! Greetings!&lt;/P&gt;&lt;P&gt;I posted following query to NXP "Wireless Connectivity" discussion portal. I am not sure if it was appropriate place for my question. Hence posting it again here (in "other NXP solutions". Hopefully it covers RF too). Please go through it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have started working on SA612A mixer. Since many days, I have been struggling in generating IF (KHz) output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP SA612A pin description (A quick reference so that you don't have to refer to the datasheet):&lt;/P&gt;&lt;P&gt;Pin1,2: differential RF input pins&lt;/P&gt;&lt;P&gt;Pin3: Ground&lt;/P&gt;&lt;P&gt;Pin4,5: differential IF output pins&lt;/P&gt;&lt;P&gt;Pin6,7: LO differential input&lt;/P&gt;&lt;P&gt;Pin8: +5V&lt;/P&gt;&lt;P&gt;My circuit configuration and problem detail:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;44.94MHz RF applied to pin1 through DC blocking capacitor. Pin2 is grounded via capacitor. RF signal level on pin1 is: &amp;lt;-15dBm (200mV peak to peak into 1.5kOhm input resistance of SA612) (&amp;lt;-15dBm ensures linear operating range considering IIP3) (at later stage I decreased the RF power further to 20mV rms, to make it operate in linear range)&lt;/LI&gt;&lt;LI&gt;44.88MHz LO applied to pin 6, pin7 left open as suggested in datasheet/ application note:AN1993. LO level on pin6 is: 230mV peak to peak (as per datasheet, it has to be 200mV to 300mV peak to peak) (at later stage I also went for 224mV rms LO input)&lt;/LI&gt;&lt;LI&gt;Expecting to see 60Kz output (difference frequency) peak in the spectrum analyzer.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;60KHz signal seems totally immersed in the noise, not a peak at all, what can be the reason? Tried with other frequencies as well.&lt;/P&gt;&lt;P&gt;Please share your views on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sanket&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 13:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-in-generating-IF-KHz-using-SA612A-mixer/m-p/549951#M3691</guid>
      <dc:creator>sanketpatel2020</dc:creator>
      <dc:date>2016-07-28T13:17:44Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in generating IF(KHz) using SA612A mixer</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-in-generating-IF-KHz-using-SA612A-mixer/m-p/549952#M3692</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please create a Service request.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/381898"&gt;How I could create a Service Request?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please provide in Service request your schematics, Input and Output traces.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 05:52:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-in-generating-IF-KHz-using-SA612A-mixer/m-p/549952#M3692</guid>
      <dc:creator>andrei_skok</dc:creator>
      <dc:date>2016-08-10T05:52:09Z</dc:date>
    </item>
  </channel>
</rss>