<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question about PTN3356 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Question-about-PTN3356/m-p/507027#M3549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to design a DisplayPort to VGA converter that works from -20° C to 85° C. PTN3356 would be perfect, but it does not work below 0° C. Are there any other solutions with NXP products? Which issues could I run into if I insist working with that device below 0° C ? Is there any way of getting samples tested/qualified in the industrial temperature range?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 May 2016 13:38:11 GMT</pubDate>
    <dc:creator>lucarigazio</dc:creator>
    <dc:date>2016-05-27T13:38:11Z</dc:date>
    <item>
      <title>Question about PTN3356</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Question-about-PTN3356/m-p/507027#M3549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to design a DisplayPort to VGA converter that works from -20° C to 85° C. PTN3356 would be perfect, but it does not work below 0° C. Are there any other solutions with NXP products? Which issues could I run into if I insist working with that device below 0° C ? Is there any way of getting samples tested/qualified in the industrial temperature range?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 May 2016 13:38:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Question-about-PTN3356/m-p/507027#M3549</guid>
      <dc:creator>lucarigazio</dc:creator>
      <dc:date>2016-05-27T13:38:11Z</dc:date>
    </item>
  </channel>
</rss>