<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックNX5DV330</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/NX5DV330/m-p/494292#M3502</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm having issues with this chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Found odd behavior of the NXP switch, the output voltage is 1V less than the input if the load is Hi-Z.&lt;/P&gt;&lt;P&gt;Also found that the output voltage gets limited to 3.5V with constant load and increasing voltage.&lt;/P&gt;&lt;P&gt;I read in the datasheet that the Input and output voltages can be 0 to 5.5V, so why am I experiencing this limiting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Feb 2016 18:52:45 GMT</pubDate>
    <dc:creator>vsabino</dc:creator>
    <dc:date>2016-02-29T18:52:45Z</dc:date>
    <item>
      <title>NX5DV330</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NX5DV330/m-p/494292#M3502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm having issues with this chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Found odd behavior of the NXP switch, the output voltage is 1V less than the input if the load is Hi-Z.&lt;/P&gt;&lt;P&gt;Also found that the output voltage gets limited to 3.5V with constant load and increasing voltage.&lt;/P&gt;&lt;P&gt;I read in the datasheet that the Input and output voltages can be 0 to 5.5V, so why am I experiencing this limiting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Feb 2016 18:52:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NX5DV330/m-p/494292#M3502</guid>
      <dc:creator>vsabino</dc:creator>
      <dc:date>2016-02-29T18:52:45Z</dc:date>
    </item>
  </channel>
</rss>