<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SC16IS741A Rx (no FIFO) Tx (with FIFO) in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS741A-Rx-no-FIFO-Tx-with-FIFO/m-p/490310#M3477</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Re: SC16IS741A&lt;/P&gt;&lt;P&gt;I need to interrupt on every Rx character (no Rx FIFO needed) but also need to be able to use the Tx FIFO so I don't have to wait for each Tx character.&amp;nbsp; Is this possible with the SC16IS741A and if so, what register (and register settings) do I need to use?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 May 2016 18:00:43 GMT</pubDate>
    <dc:creator>kenstewart-smit</dc:creator>
    <dc:date>2016-05-21T18:00:43Z</dc:date>
    <item>
      <title>SC16IS741A Rx (no FIFO) Tx (with FIFO)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS741A-Rx-no-FIFO-Tx-with-FIFO/m-p/490310#M3477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Re: SC16IS741A&lt;/P&gt;&lt;P&gt;I need to interrupt on every Rx character (no Rx FIFO needed) but also need to be able to use the Tx FIFO so I don't have to wait for each Tx character.&amp;nbsp; Is this possible with the SC16IS741A and if so, what register (and register settings) do I need to use?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 May 2016 18:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS741A-Rx-no-FIFO-Tx-with-FIFO/m-p/490310#M3477</guid>
      <dc:creator>kenstewart-smit</dc:creator>
      <dc:date>2016-05-21T18:00:43Z</dc:date>
    </item>
  </channel>
</rss>