<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NX3L1G384 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/NX3L1G384/m-p/484761#M3453</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NX3L1G384.&amp;nbsp; The data sheet for this switch suggests a clamp diode on the signal leads.&amp;nbsp; First, is the clamp diode on both sides so that the input and output are both clamped regardless of switch condition?&amp;nbsp; If clamp is one side only, then which side?&amp;nbsp; Spec indicates a -50mA current clamp, and implies a -0.5V clamp voltage.&amp;nbsp; This voltage and current are for signals that extend below ground, yes?&amp;nbsp; If my signal is AC coupled into the switch, with a ground resistor at the signal lead, and is 2V pk-pk will this signal produce clipping due to the signal swing going to -1.0V and turning on the protection diodes?&amp;nbsp; Thanks, Charles (Skip) Robidart&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Feb 2016 22:53:13 GMT</pubDate>
    <dc:creator>charlesrobidart</dc:creator>
    <dc:date>2016-02-24T22:53:13Z</dc:date>
    <item>
      <title>NX3L1G384</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NX3L1G384/m-p/484761#M3453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NX3L1G384.&amp;nbsp; The data sheet for this switch suggests a clamp diode on the signal leads.&amp;nbsp; First, is the clamp diode on both sides so that the input and output are both clamped regardless of switch condition?&amp;nbsp; If clamp is one side only, then which side?&amp;nbsp; Spec indicates a -50mA current clamp, and implies a -0.5V clamp voltage.&amp;nbsp; This voltage and current are for signals that extend below ground, yes?&amp;nbsp; If my signal is AC coupled into the switch, with a ground resistor at the signal lead, and is 2V pk-pk will this signal produce clipping due to the signal swing going to -1.0V and turning on the protection diodes?&amp;nbsp; Thanks, Charles (Skip) Robidart&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Feb 2016 22:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NX3L1G384/m-p/484761#M3453</guid>
      <dc:creator>charlesrobidart</dc:creator>
      <dc:date>2016-02-24T22:53:13Z</dc:date>
    </item>
  </channel>
</rss>