<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CWH-CTP-BASE-HE stuck at solid red TX/RX LED – no USB enumeration or Ethernet link in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/CWH-CTP-BASE-HE-stuck-at-solid-red-TX-RX-LED-no-USB-enumeration/m-p/2409064#M33258</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I recently purchased a CodeWarrior TAP CWH-CTP-BASE-HE, but I am unable to get it working.&lt;/P&gt;&lt;P&gt;Current condition:&lt;/P&gt;&lt;P&gt;TX/RX LED stays continuously solid red.&lt;/P&gt;&lt;P&gt;Nothing appears in Windows Device Manager when I connect or disconnect the TAP through USB.&lt;/P&gt;&lt;P&gt;I have tried different USB cables and different USB ports.&lt;/P&gt;&lt;P&gt;I also connected the Ethernet port to a working switch/router while USB was connected for power.&lt;/P&gt;&lt;P&gt;The Ethernet Link LED does not turn on.&lt;/P&gt;&lt;P&gt;There is currently no target processor, target board, or probe tip connected.&lt;/P&gt;&lt;P&gt;My unit does not appear to have an external reset button.&lt;/P&gt;&lt;P&gt;From the CodeWarrior TAP documentation, I understand that the TX/RX LED should normally change from red to flashing orange and then flashing green when the TAP boots successfully. In my case it stays permanently solid red.&lt;/P&gt;&lt;P&gt;Could you please advise:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Does a permanently solid red TX/RX LED mean that the TAP bootloader or operating system is not starting correctly?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Could this be caused by a missing USB driver even though the Ethernet Link LED is also not working?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there any recovery or bootloader mode available for the CWH-CTP-BASE-HE if both USB and Ethernet communication are unavailable?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there an internal JTAG or programming connector that can be used to recover the TAP firmware?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is a recovery firmware image or recovery utility available from NXP?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there any additional diagnostic procedure I should perform before considering the unit faulty?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I can provide the hardware revision, serial number, photographs of the unit, and PCB photographs if required.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Fri, 28 Aug 2026 04:27:09 GMT</pubDate>
    <dc:creator>apusen</dc:creator>
    <dc:date>2026-08-28T04:27:09Z</dc:date>
    <item>
      <title>CWH-CTP-BASE-HE stuck at solid red TX/RX LED – no USB enumeration or Ethernet link</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CWH-CTP-BASE-HE-stuck-at-solid-red-TX-RX-LED-no-USB-enumeration/m-p/2409064#M33258</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I recently purchased a CodeWarrior TAP CWH-CTP-BASE-HE, but I am unable to get it working.&lt;/P&gt;&lt;P&gt;Current condition:&lt;/P&gt;&lt;P&gt;TX/RX LED stays continuously solid red.&lt;/P&gt;&lt;P&gt;Nothing appears in Windows Device Manager when I connect or disconnect the TAP through USB.&lt;/P&gt;&lt;P&gt;I have tried different USB cables and different USB ports.&lt;/P&gt;&lt;P&gt;I also connected the Ethernet port to a working switch/router while USB was connected for power.&lt;/P&gt;&lt;P&gt;The Ethernet Link LED does not turn on.&lt;/P&gt;&lt;P&gt;There is currently no target processor, target board, or probe tip connected.&lt;/P&gt;&lt;P&gt;My unit does not appear to have an external reset button.&lt;/P&gt;&lt;P&gt;From the CodeWarrior TAP documentation, I understand that the TX/RX LED should normally change from red to flashing orange and then flashing green when the TAP boots successfully. In my case it stays permanently solid red.&lt;/P&gt;&lt;P&gt;Could you please advise:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Does a permanently solid red TX/RX LED mean that the TAP bootloader or operating system is not starting correctly?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Could this be caused by a missing USB driver even though the Ethernet Link LED is also not working?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there any recovery or bootloader mode available for the CWH-CTP-BASE-HE if both USB and Ethernet communication are unavailable?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there an internal JTAG or programming connector that can be used to recover the TAP firmware?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is a recovery firmware image or recovery utility available from NXP?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there any additional diagnostic procedure I should perform before considering the unit faulty?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I can provide the hardware revision, serial number, photographs of the unit, and PCB photographs if required.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Aug 2026 04:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CWH-CTP-BASE-HE-stuck-at-solid-red-TX-RX-LED-no-USB-enumeration/m-p/2409064#M33258</guid>
      <dc:creator>apusen</dc:creator>
      <dc:date>2026-08-28T04:27:09Z</dc:date>
    </item>
    <item>
      <title>Re: CWH-CTP-BASE-HE stuck at solid red TX/RX LED – no USB enumeration or Ethernet link</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CWH-CTP-BASE-HE-stuck-at-solid-red-TX-RX-LED-no-USB-enumeration/m-p/2409099#M33259</link>
      <description>&lt;P&gt;Please download the attached ccs.zip file and install CCS USB driver from&amp;nbsp;&lt;/P&gt;
&lt;P&gt;C:\Users\nxa22585\Downloads\260821\ccs\ccs\ccs\drivers\usb\x64&lt;/P&gt;
&lt;P&gt;Please don't plugin CodeWarrior TAP when installing the driver.&lt;/P&gt;
&lt;P&gt;Then plug in CodeWarrior TAP and check the device manager whether you can find CodeWarrior TAP information similar as the attachment.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Aug 2026 07:57:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CWH-CTP-BASE-HE-stuck-at-solid-red-TX-RX-LED-no-USB-enumeration/m-p/2409099#M33259</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-08-28T07:57:16Z</dc:date>
    </item>
    <item>
      <title>Re: CWH-CTP-BASE-HE stuck at solid red TX/RX LED – no USB enumeration or Ethernet link</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CWH-CTP-BASE-HE-stuck-at-solid-red-TX-RX-LED-no-USB-enumeration/m-p/2409273#M33260</link>
      <description>&lt;P&gt;Is it compatible with Windows 11? I have installed into win 11 but still same as before not showing into device manager .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Aug 2026 16:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CWH-CTP-BASE-HE-stuck-at-solid-red-TX-RX-LED-no-USB-enumeration/m-p/2409273#M33260</guid>
      <dc:creator>apusen</dc:creator>
      <dc:date>2026-08-28T16:45:57Z</dc:date>
    </item>
    <item>
      <title>Re: CWH-CTP-BASE-HE stuck at solid red TX/RX LED – no USB enumeration or Ethernet link</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CWH-CTP-BASE-HE-stuck-at-solid-red-TX-RX-LED-no-USB-enumeration/m-p/2409568#M33268</link>
      <description>&lt;P&gt;Yes, it is&amp;nbsp;&lt;SPAN&gt;compatible with Windows 11.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;It seems that there is problem with your CodeWarrior TAP, you could return this CodeWarrior TAP and replace it for a new one from the following link.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/support/sample-and-buy/how-to-buy-from-nxp/dev-tool-warranty-return-request-form:WTB_DTD_WARRANTY" target="_blank"&gt;https://www.nxp.com/support/sample-and-buy/how-to-buy-from-nxp/dev-tool-warranty-return-request-form:WTB_DTD_WARRANTY&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 31 Aug 2026 08:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CWH-CTP-BASE-HE-stuck-at-solid-red-TX-RX-LED-no-USB-enumeration/m-p/2409568#M33268</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-08-31T08:29:36Z</dc:date>
    </item>
  </channel>
</rss>