<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Productsのトピックls1021a eTSEC tx timeout</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2397364#M32978</link>
    <description>&lt;P&gt;I have a LS1021A IOT and a prototype board based on this cpu. On both we use our boot loader.&lt;/P&gt;&lt;P&gt;It works perfectly in the IOT board but on my board I get TX timeout on the Ethernet port. I get a few pings going and then tx timeout and more pings.&amp;nbsp; This makes tftp rarely possible.&lt;/P&gt;&lt;P&gt;There are hardware difference of course. Our MAC is connected to a BCM54616S then to a LAN9514. The autonegotiation is limited to 100FD. TX timeout also happens in loopback mode.&lt;/P&gt;&lt;P&gt;In order to transmit data, I had to set bit SGMII_AN bit in the TBI PHY on my boards while I did not have to on the IOT (IOT can negotiate at 1000FD).&lt;/P&gt;&lt;P&gt;Not sure why the TX is so intermittent. Could it be related to this speed limitation?&lt;/P&gt;</description>
    <pubDate>Tue, 21 Jul 2026 15:32:02 GMT</pubDate>
    <dc:creator>renaud</dc:creator>
    <dc:date>2026-07-21T15:32:02Z</dc:date>
    <item>
      <title>ls1021a eTSEC tx timeout</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2397364#M32978</link>
      <description>&lt;P&gt;I have a LS1021A IOT and a prototype board based on this cpu. On both we use our boot loader.&lt;/P&gt;&lt;P&gt;It works perfectly in the IOT board but on my board I get TX timeout on the Ethernet port. I get a few pings going and then tx timeout and more pings.&amp;nbsp; This makes tftp rarely possible.&lt;/P&gt;&lt;P&gt;There are hardware difference of course. Our MAC is connected to a BCM54616S then to a LAN9514. The autonegotiation is limited to 100FD. TX timeout also happens in loopback mode.&lt;/P&gt;&lt;P&gt;In order to transmit data, I had to set bit SGMII_AN bit in the TBI PHY on my boards while I did not have to on the IOT (IOT can negotiate at 1000FD).&lt;/P&gt;&lt;P&gt;Not sure why the TX is so intermittent. Could it be related to this speed limitation?&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jul 2026 15:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2397364#M32978</guid>
      <dc:creator>renaud</dc:creator>
      <dc:date>2026-07-21T15:32:02Z</dc:date>
    </item>
    <item>
      <title>Re: ls1021a eTSEC tx timeout</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2397366#M32979</link>
      <description>Forgot to say my port is set for SGMII mode.</description>
      <pubDate>Tue, 21 Jul 2026 15:58:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2397366#M32979</guid>
      <dc:creator>renaud</dc:creator>
      <dc:date>2026-07-21T15:58:09Z</dc:date>
    </item>
    <item>
      <title>Re: ls1021a eTSEC tx timeout</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2397390#M32981</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class=""&gt;For 100FD SGMII , verify these items in your boot loader on the prototype board:&lt;/P&gt;
&lt;OL class=""&gt;
&lt;LI class="" style="list-style-type: disc;"&gt;
&lt;P class=""&gt;Set LS1021A eTSEC for SGMII 100 Mbps&lt;/P&gt;
&lt;UL class=""&gt;
&lt;LI class="" style="list-style-type: disc;"&gt;&lt;CODE class=""&gt;ECNTRL[TBIM] = 1&lt;/CODE&gt;&lt;/LI&gt;
&lt;LI class="" style="list-style-type: disc;"&gt;&lt;CODE class=""&gt;ECNTRL[SGMIIM] = 1&lt;/CODE&gt;&lt;/LI&gt;
&lt;LI class="" style="list-style-type: disc;"&gt;&lt;CODE class=""&gt;ECNTRL[R100M] = 1&lt;/CODE&gt;&lt;/LI&gt;
&lt;LI class="" style="list-style-type: disc;"&gt;&lt;CODE class=""&gt;MACCFG2[I/F Mode] = 01&lt;/CODE&gt; for 10/100 mode&lt;BR /&gt;The LS1021A RM specifically notes setting &lt;CODE class=""&gt;R100M = 1&lt;/CODE&gt; for SGMII 100 Mbps.&lt;/LI&gt;
&lt;/UL&gt;
&lt;/LI&gt;
&lt;LI class="" style="list-style-type: disc;"&gt;
&lt;P class=""&gt;Reset and program the internal TBI PHY The RM states that SGMII uses the TBI register set and that it is important to reset the TBI for all interface modes, including SGMII.&lt;/P&gt;
&lt;/LI&gt;
&lt;LI class="" style="list-style-type: disc;"&gt;
&lt;P class=""&gt;Keep &lt;CODE class=""&gt;SGMII_AN&lt;/CODE&gt; set The TBI &lt;CODE class=""&gt;SGMII_AN&lt;/CODE&gt; bit is documented as “must be set to 1.” So the fact that your board only transmits after setting this bit is not surprising; it suggests your boot-loader initialization was incomplete for this PHY/MAC mode.&lt;/P&gt;
&lt;/LI&gt;
&lt;LI class="" style="list-style-type: disc;"&gt;
&lt;P class=""&gt;Do not rely on 1G-style SGMII AN behavior at 100 Mbps There are known LS1021A reports where 100 Mbps SGMII operation shows “SGMII link is not ok” or intermittent no-packet behavior after link cycling, while 1G operation is clean. That does not prove your exact TX timeout root cause, but it makes 100FD SGMII configuration a strong suspect.&lt;/P&gt;
&lt;/LI&gt;
&lt;/OL&gt;
&lt;P class=""&gt;The loopback result matters. If your “loopback mode” is external PHY loopback or SGMII-side loopback, the 100FD SGMII/TBI setup can still be involved. If it is internal MAC/eTSEC loopback , then the external BCM54616S/LAN9514 path is mostly out of the picture, and I would focus on eTSEC initialization, descriptor-ring handling, cache coherency, and TX halt/error status.&lt;/P&gt;
&lt;P class=""&gt;For debugging, check the eTSEC TX halt status when the timeout occurs. The RM says the transmit halt bits are set when eTSEC is no longer processing transmit frames from a TxBD ring; repeatable causes include bus errors, invalid BD/data addresses, uncorrectable BD/data read errors, and TxBD programming errors such as &lt;CODE class=""&gt;Ready = 1&lt;/CODE&gt; with length &lt;CODE class=""&gt;0&lt;/CODE&gt; . Also check whether you are seeing &lt;CODE class=""&gt;IEVENT_BSY&lt;/CODE&gt; ; NXP material describes BSY as dropped RX frames due to lack of buffers/software not servicing the BD ring fast enough, which is a software/BD-ring symptom rather than a pure SGMII electrical symptom.&lt;/P&gt;
&lt;P class=""&gt;Recommended isolation sequence:&lt;/P&gt;
&lt;DIV class="text-left mx-auto flex h-full min-h-0 w-full"&gt;
&lt;DIV class="relative size-full overflow-auto rounded-none border border-border shadow-lg"&gt;
&lt;PRE style="background-color: var(--code-bg, #fafafa); background-position: 0% 0%; background-repeat: repeat; background-attachment: scroll; background-image: none; background-size: auto; background-origin: padding-box; background-clip: border-box; color: #383a42; font-family: 'Fira Code', 'Fira Mono', Menlo, Consolas, 'DejaVu Sans Mono', monospace; direction: ltr; text-align: left; white-space: pre; word-spacing: normal; word-break: normal; line-height: 1.5; tab-size: 2; hyphens: none; padding: 1rem; margin: 0px; overflow: auto; border-radius: 0px; width: 100%; font-size: 0.875rem;"&gt;&lt;CODE class="language-javascript" style="white-space: pre; background: #fafafa; color: #383a42; font-family: 'Fira Code', 'Fira Mono', Menlo, Consolas, 'DejaVu Sans Mono', monospace; direction: ltr; text-align: left; word-spacing: normal; word-break: normal; line-height: 1.5; tab-size: 2; hyphens: none;"&gt;&lt;SPAN class="token"&gt;1.&lt;/SPAN&gt; &lt;SPAN class="token maybe-class-name"&gt;Force&lt;/SPAN&gt; external &lt;SPAN class="token"&gt;PHY&lt;/SPAN&gt; to 100FD&lt;SPAN class="token"&gt;,&lt;/SPAN&gt; no autoneg toward copper &lt;SPAN class="token control-flow"&gt;if&lt;/SPAN&gt; needed&lt;SPAN class="token"&gt;.&lt;/SPAN&gt;
&lt;SPAN class="token"&gt;2.&lt;/SPAN&gt; &lt;SPAN class="token maybe-class-name"&gt;Force&lt;/SPAN&gt; &lt;SPAN class="token"&gt;LS1021A&lt;/SPAN&gt; &lt;SPAN class="token"&gt;MAC&lt;/SPAN&gt;&lt;SPAN class="token"&gt;/&lt;/SPAN&gt;eTSEC to &lt;SPAN class="token"&gt;SGMII&lt;/SPAN&gt; &lt;SPAN class="token"&gt;100&lt;/SPAN&gt; &lt;SPAN class="token literal-property"&gt;Mbps&lt;/SPAN&gt;&lt;SPAN class="token"&gt;:&lt;/SPAN&gt;
   &lt;SPAN class="token"&gt;TBIM&lt;/SPAN&gt;&lt;SPAN class="token"&gt;=&lt;/SPAN&gt;&lt;SPAN class="token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="token"&gt;SGMIIM&lt;/SPAN&gt;&lt;SPAN class="token"&gt;=&lt;/SPAN&gt;&lt;SPAN class="token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="token"&gt;R100M&lt;/SPAN&gt;&lt;SPAN class="token"&gt;=&lt;/SPAN&gt;&lt;SPAN class="token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="token"&gt;MACCFG2&lt;/SPAN&gt; &lt;SPAN class="token"&gt;I&lt;/SPAN&gt;&lt;SPAN class="token"&gt;/&lt;/SPAN&gt;&lt;SPAN class="token"&gt;F&lt;/SPAN&gt; mode&lt;SPAN class="token"&gt;=&lt;/SPAN&gt;&lt;SPAN class="token"&gt;10&lt;/SPAN&gt;&lt;SPAN class="token"&gt;/&lt;/SPAN&gt;&lt;SPAN class="token"&gt;100.&lt;/SPAN&gt;
&lt;SPAN class="token"&gt;3.&lt;/SPAN&gt; &lt;SPAN class="token maybe-class-name"&gt;Reset&lt;/SPAN&gt;&lt;SPAN class="token"&gt;/&lt;/SPAN&gt;reinitialize &lt;SPAN class="token"&gt;TBI&lt;/SPAN&gt; after setting &lt;SPAN class="token"&gt;SGMII&lt;/SPAN&gt; mode&lt;SPAN class="token"&gt;.&lt;/SPAN&gt;
&lt;SPAN class="token"&gt;4.&lt;/SPAN&gt; &lt;SPAN class="token known-class-name"&gt;Set&lt;/SPAN&gt; &lt;SPAN class="token"&gt;TBI&lt;/SPAN&gt; &lt;SPAN class="token"&gt;SGMII_AN&lt;/SPAN&gt;&lt;SPAN class="token"&gt;=&lt;/SPAN&gt;&lt;SPAN class="token"&gt;1.&lt;/SPAN&gt;
&lt;SPAN class="token"&gt;5.&lt;/SPAN&gt; &lt;SPAN class="token maybe-class-name"&gt;Confirm&lt;/SPAN&gt; &lt;SPAN class="token"&gt;TBI&lt;/SPAN&gt; link&lt;SPAN class="token"&gt;/&lt;/SPAN&gt;&lt;SPAN class="token"&gt;AN&lt;/SPAN&gt; status&lt;SPAN class="token"&gt;,&lt;/SPAN&gt; eTSEC &lt;SPAN class="token"&gt;ECNTRL&lt;/SPAN&gt;&lt;SPAN class="token"&gt;/&lt;/SPAN&gt;&lt;SPAN class="token"&gt;MACCFG2&lt;/SPAN&gt;&lt;SPAN class="token"&gt;,&lt;/SPAN&gt; and &lt;SPAN class="token"&gt;PHY&lt;/SPAN&gt; &lt;SPAN class="token"&gt;SGMII&lt;/SPAN&gt;&lt;SPAN class="token"&gt;-&lt;/SPAN&gt;side status&lt;SPAN class="token"&gt;.&lt;/SPAN&gt;
&lt;SPAN&gt;&lt;SPAN class="token"&gt;6.&lt;/SPAN&gt; &lt;SPAN class="token maybe-class-name"&gt;On&lt;/SPAN&gt; timeout&lt;SPAN class="token"&gt;,&lt;/SPAN&gt; dump &lt;SPAN class="token"&gt;IEVENT&lt;/SPAN&gt;&lt;SPAN class="token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="token"&gt;TX&lt;/SPAN&gt; halt registers&lt;SPAN class="token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="token"&gt;DMA&lt;/SPAN&gt; status&lt;SPAN class="token"&gt;,&lt;/SPAN&gt; and &lt;SPAN class="token"&gt;TXBD&lt;/SPAN&gt; ring contents&lt;SPAN class="token"&gt;.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;regards&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jul 2026 18:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2397390#M32981</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2026-07-21T18:19:10Z</dc:date>
    </item>
    <item>
      <title>Re: ls1021a eTSEC tx timeout</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2398138#M32995</link>
      <description>&lt;P&gt;Adding messages or 1ms delay in the send functions allows the correct transfer of data without loss.&lt;/P&gt;&lt;P&gt;I added a DMA flush to the TX descriptors in the send function and this helps. Though, this should not be necessary considering the descriptors are allocated in uncached memory. It could be a defect in the MMU library to which I added LPAE support.&lt;/P&gt;&lt;P&gt;Now I remember that a long time ago I removed the dma-coherent property in the enet device node and this was enough for the LS1021A-IOT to work. This is forcing a DMA flush while allocating uncached memory for the descriptors. But there was no cache flush in the send functions which updates the TX descriptors on each packet. Not sure why it does not work on my prototype (difference in frequency, DDR3L vs DDR4,...)&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jul 2026 09:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2398138#M32995</guid>
      <dc:creator>renaud</dc:creator>
      <dc:date>2026-07-23T09:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: ls1021a eTSEC tx timeout</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2398439#M33007</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea" data-pm-slice="1 1 []"&gt;Thank you for the detailed findings — the combination of workarounds you identified (1 ms delay, manual DMA flush, and removing &lt;CODE&gt;dma-coherent&lt;/CODE&gt;) is a textbook fingerprint of a cache alias problem. Here is the root cause explanation and the recommended fix path.&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;&lt;STRONG&gt;Root cause: cached virtual alias over the TX descriptor region&lt;/STRONG&gt;&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;The LS1021A ENET DMA is a non-cache-coherent bus master — it reads DDR directly, with no visibility into the CPU cache. The correct operating model for gianfar on LS1021A is the non-coherent software-managed model: descriptors allocated in uncached memory, with explicit &lt;CODE&gt;dma_sync_*&lt;/CODE&gt; calls whenever the CPU updates a descriptor field.&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;What your LPAE changes most likely introduced is a page table entry for the descriptor physical address range that carries the wrong cache attribute — Normal Writeback instead of Device or Normal Non-cacheable. This creates two virtual aliases to the same physical memory with different cacheability: the allocation path (via &lt;CODE&gt;dma_alloc_noncoherent&lt;/CODE&gt;) maps it uncached, but the per-packet TX descriptor update path in the send function accesses it through a cached alias. The CPU writes the updated descriptor fields into the cache line, they never reach DDR, and the ENET DMA reads stale data and underruns.&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;&lt;STRONG&gt;Why your three workarounds all mask the same defect&lt;/STRONG&gt;&lt;/P&gt;
&lt;UL class="wnfdntf" dir="auto"&gt;
&lt;LI class="wnfdnte _1ibi0s33w" dir="auto"&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;1 ms delay / message insertion: adds enough latency for the CPU writeback buffer to drain naturally under low load — timing-dependent, will fail under traffic or frequency change.&lt;/P&gt;
&lt;/LI&gt;
&lt;LI class="wnfdnte _1ibi0s33w" dir="auto"&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;Manual &lt;CODE&gt;dma_flush&lt;/CODE&gt; in the send function: forces a cache clean-to-PoC before the DMA reads the descriptor — correct behaviour, but should not be necessary if the region is genuinely uncached.&lt;/P&gt;
&lt;/LI&gt;
&lt;LI class="wnfdnte _1ibi0s33w" dir="auto"&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;Removing &lt;CODE&gt;dma-coherent&lt;/CODE&gt; from the enet device node: causes the kernel to call &lt;CODE&gt;dma_map_single()&lt;/CODE&gt; / &lt;CODE&gt;dma_sync_single_for_device()&lt;/CODE&gt; on each TX descriptor before submission, which explicitly cleans the cache — also correct, and explains why the LS1021A-IOT worked reliably without a send-path flush.&lt;/P&gt;
&lt;/LI&gt;
&lt;/UL&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;The absence of the send-path flush is the missing piece. The LS1021A-IOT worked with &lt;CODE&gt;dma-coherent&lt;/CODE&gt; removed because the kernel's DMA mapping layer inserted the sync automatically; your prototype does not have that path because the LPAE changes altered the descriptor region's cache attributes without re-introducing the sync.&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;&lt;STRONG&gt;DDR3L vs DDR4 / frequency difference&lt;/STRONG&gt;&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;This is not the root cause. Different DRAM type and frequency change write latency and buffer drain timing, which is why the failure is more visible on your prototype — but the underlying defect is architectural and will be present on both boards under sufficient load.&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;&lt;STRONG&gt;Recommended fix&lt;/STRONG&gt;&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;The correct and self-consistent fix is to combine both of the following:&lt;/P&gt;
&lt;OL class="wnfdntg" dir="auto"&gt;
&lt;LI class="wnfdnte _1ibi0s33w" dir="auto"&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;Keep &lt;CODE&gt;dma-coherent&lt;/CODE&gt; removed from the enet device node (non-coherent model). This causes the kernel DMA layer to issue &lt;CODE&gt;dma_sync_single_for_device()&lt;/CODE&gt; automatically before DMA ownership is transferred for descriptors allocated via &lt;CODE&gt;dma_alloc_noncoherent&lt;/CODE&gt;.&lt;/P&gt;
&lt;/LI&gt;
&lt;LI class="wnfdnte _1ibi0s33w" dir="auto"&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;Add explicit &lt;CODE&gt;dma_sync_single_for_device()&lt;/CODE&gt; calls in the TX send path at the point where TX descriptor fields (&lt;CODE&gt;status&lt;/CODE&gt;, &lt;CODE&gt;data_length&lt;/CODE&gt;, &lt;CODE&gt;data_pointer&lt;/CODE&gt;) are written on each packet. This is the flush you added manually — but it should be formally placed as a &lt;CODE&gt;dma_sync_single_for_device(dev, desc_dma_addr, sizeof(txbd), DMA_TO_DEVICE)&lt;/CODE&gt; before writing &lt;CODE&gt;TDAR&lt;/CODE&gt;. This makes the model explicit and correct regardless of how the MMU attributes the descriptor region.&lt;/P&gt;
&lt;/LI&gt;
&lt;LI class="wnfdnte _1ibi0s33w" dir="auto"&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;Separately, audit the LPAE MMU library change for the &lt;CODE&gt;AttrIndx&lt;/CODE&gt; / &lt;CODE&gt;TEX+C+B&lt;/CODE&gt; fields assigned to the physical address range used for ENET descriptors. The descriptor pool should be mapped as Device-nGnRnE (strongly ordered) or Normal Non-cacheable — not Normal Writeback. You can verify the actual attributes in use with the kernel's &lt;CODE&gt;ptdump&lt;/CODE&gt; debug interface by checking the virtual address of the descriptor pool after allocation.&lt;/P&gt;
&lt;/LI&gt;
&lt;/OL&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;The DMA flush you added is not a workaround — it is the correct mechanism. The real defect is that it was absent from the send path in the first place, and the LPAE changes exposed this because they altered the effective cacheability of the region.&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P class="wnfdntu _1ibi0s3f5 _1ibi0s3ce _1ibi0s3ea"&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jul 2026 18:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/ls1021a-eTSEC-tx-timeout/m-p/2398439#M33007</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2026-07-23T18:24:53Z</dc:date>
    </item>
  </channel>
</rss>