<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: IO Expansion for LEDs</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/IO-Expansion-for-LEDs/m-p/2396668#M32948</link>
    <description>&lt;DIV&gt;PCAL6524 is well suited for driving a large number of optical relays and LEDs. However, the Agile I/O drive strength is not intended to replace the required series current-limiting resistors. To mitigate the risk of unintended current during power-up when the I/Os are still in their input state, options such as using a 3.3 V LED supply with a lower VDD(P), or implementing a global LED power switch, may be considered. Nevertheless, individual current-limiting resistors should always be retained for each LED channel.&lt;/DIV&gt;</description>
    <pubDate>Mon, 20 Jul 2026 06:37:31 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2026-07-20T06:37:31Z</dc:date>
    <item>
      <title>IO Expansion for LEDs</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IO-Expansion-for-LEDs/m-p/2395936#M32917</link>
      <description>&lt;P&gt;I am currently designing on a switch matrix board for custom measurement equipment.&lt;BR /&gt;To route the signals I plan on using optical relays, the G3VM-61DR1 to be precise.&lt;BR /&gt;So I need to control &amp;gt;250! LEDs (1,5-1,8V 6-8mA) somehow.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Only &amp;lt;25 will be turned on at the same time&lt;/LI&gt;&lt;LI&gt;Supply voltage will be 3.3V or lower, temperature should be around 40°C&lt;/LI&gt;&lt;LI&gt;We just need to turn them on or off, no dimming or PWM&lt;/LI&gt;&lt;LI&gt;I don't want to use an LED driver because of the noise it might/will introduce&lt;/LI&gt;&lt;LI&gt;I can't use a classic matrix arrangement since it is unknown which switches will be on at the same time&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;So the only option is to have a discrete output for each relay/LED, your IO Expanders look promising for this, eg. the &lt;LI-PRODUCT title="PCAL6524" id="PCAL6524"&gt;&lt;/LI-PRODUCT&gt;.&lt;/P&gt;&lt;P&gt;Because of the high channel count I want to reduce the components per channel as much as possible, so I have some questions:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Can I rely on the 7,5mA current setting of the Agile IO devices and omit the LED series resistor?&lt;/LI&gt;&lt;LI&gt;If this is ok, what are possible side effects?&lt;/LI&gt;&lt;LI&gt;Since the devices start configured as Input some experience high currents when they are used to control LEDs(eg.&amp;nbsp;&lt;LI-PRODUCT title="PCA9535A" id="PCA9535A"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp; Datasheet page 14/15). The classic fix with a pullup for each channel is not cool for so many channels. Does this also affect the Agile IO devices?&lt;/LI&gt;&lt;LI&gt;Can this be circumvented by supplying the LEDs with 3.3V and the expanders with 1.65V?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;P&gt;Otto&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jul 2026 10:51:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IO-Expansion-for-LEDs/m-p/2395936#M32917</guid>
      <dc:creator>0tto</dc:creator>
      <dc:date>2026-07-16T10:51:15Z</dc:date>
    </item>
    <item>
      <title>Re: IO Expansion for LEDs</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IO-Expansion-for-LEDs/m-p/2396668#M32948</link>
      <description>&lt;DIV&gt;PCAL6524 is well suited for driving a large number of optical relays and LEDs. However, the Agile I/O drive strength is not intended to replace the required series current-limiting resistors. To mitigate the risk of unintended current during power-up when the I/Os are still in their input state, options such as using a 3.3 V LED supply with a lower VDD(P), or implementing a global LED power switch, may be considered. Nevertheless, individual current-limiting resistors should always be retained for each LED channel.&lt;/DIV&gt;</description>
      <pubDate>Mon, 20 Jul 2026 06:37:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IO-Expansion-for-LEDs/m-p/2396668#M32948</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2026-07-20T06:37:31Z</dc:date>
    </item>
  </channel>
</rss>