<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックIW612 Bluetooth RF Test</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/IW612-Bluetooth-RF-Test/m-p/2396091#M32924</link>
    <description>&lt;P&gt;Hello everyone,&lt;BR /&gt;&lt;BR /&gt;I'm trying to execute the RF Test for the module based on IW612. For this, I followed a couple of documents, such as:&lt;BR /&gt;&lt;BR /&gt;AN14310 - NXP Bluetooth UART Driver Integration&lt;BR /&gt;AN14114 -&amp;nbsp;RF Test Mode on Linux OS&lt;BR /&gt;AN14163 -&amp;nbsp;Bluetooth Direct Test Mode&lt;BR /&gt;&lt;BR /&gt;And others.&lt;BR /&gt;I'm facing some problems:&lt;BR /&gt;- In Wi-fi 5 GHz, I'm not able to see waveforms generated for low channels, near to 5 GHz, only for higher channels&amp;nbsp;&lt;BR /&gt;- For Bluetooth, I'm not able to generate waveforms for the classic Bluetooth, only for BLE (commands for scan and get the pair information using hcitool work fine, hence I don't think this is a Hardware issue)&lt;BR /&gt;&lt;BR /&gt;In my setup, I'm using the SoM Variscite Dart IMX8M (version 2.0), with a 2EL radio, based on IW612. To get the waveforms, I'm using HackRF.&lt;BR /&gt;&lt;BR /&gt;I'm using the system with Kernel 6.6.23, Yocto custom version, and with Firmware&amp;nbsp;sduart_nw61x_v1.bin.se, default from the version&lt;BR /&gt;&lt;BR /&gt;The feedback for the HCI commands is compatible with the documents, but I can't see the waveforms. May you help me if I'm missing something in our system or procedures to generate it? This is part of the Certification process, and now I'm stuck on it.&lt;BR /&gt;&lt;BR /&gt;THanks very much&lt;/P&gt;</description>
    <pubDate>Thu, 16 Jul 2026 20:55:56 GMT</pubDate>
    <dc:creator>HelbertPaulino</dc:creator>
    <dc:date>2026-07-16T20:55:56Z</dc:date>
    <item>
      <title>IW612 Bluetooth RF Test</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IW612-Bluetooth-RF-Test/m-p/2396091#M32924</link>
      <description>&lt;P&gt;Hello everyone,&lt;BR /&gt;&lt;BR /&gt;I'm trying to execute the RF Test for the module based on IW612. For this, I followed a couple of documents, such as:&lt;BR /&gt;&lt;BR /&gt;AN14310 - NXP Bluetooth UART Driver Integration&lt;BR /&gt;AN14114 -&amp;nbsp;RF Test Mode on Linux OS&lt;BR /&gt;AN14163 -&amp;nbsp;Bluetooth Direct Test Mode&lt;BR /&gt;&lt;BR /&gt;And others.&lt;BR /&gt;I'm facing some problems:&lt;BR /&gt;- In Wi-fi 5 GHz, I'm not able to see waveforms generated for low channels, near to 5 GHz, only for higher channels&amp;nbsp;&lt;BR /&gt;- For Bluetooth, I'm not able to generate waveforms for the classic Bluetooth, only for BLE (commands for scan and get the pair information using hcitool work fine, hence I don't think this is a Hardware issue)&lt;BR /&gt;&lt;BR /&gt;In my setup, I'm using the SoM Variscite Dart IMX8M (version 2.0), with a 2EL radio, based on IW612. To get the waveforms, I'm using HackRF.&lt;BR /&gt;&lt;BR /&gt;I'm using the system with Kernel 6.6.23, Yocto custom version, and with Firmware&amp;nbsp;sduart_nw61x_v1.bin.se, default from the version&lt;BR /&gt;&lt;BR /&gt;The feedback for the HCI commands is compatible with the documents, but I can't see the waveforms. May you help me if I'm missing something in our system or procedures to generate it? This is part of the Certification process, and now I'm stuck on it.&lt;BR /&gt;&lt;BR /&gt;THanks very much&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jul 2026 20:55:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IW612-Bluetooth-RF-Test/m-p/2396091#M32924</guid>
      <dc:creator>HelbertPaulino</dc:creator>
      <dc:date>2026-07-16T20:55:56Z</dc:date>
    </item>
    <item>
      <title>Re: IW612 Bluetooth RF Test</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IW612-Bluetooth-RF-Test/m-p/2396161#M32927</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you share test cmd and result screen shot to us?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Shaun&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jul 2026 02:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IW612-Bluetooth-RF-Test/m-p/2396161#M32927</guid>
      <dc:creator>shaun_wu</dc:creator>
      <dc:date>2026-07-17T02:45:00Z</dc:date>
    </item>
    <item>
      <title>Re: IW612 Bluetooth RF Test</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/IW612-Bluetooth-RF-Test/m-p/2396468#M32933</link>
      <description>&lt;P&gt;Hello Shaun,&lt;BR /&gt;&lt;BR /&gt;Sure. I ran these commands for hcitool and for wifi, I attached the final file for the config&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;For Bluetooth Classic&lt;BR /&gt;------------------------------------&lt;BR /&gt;THESE COMMANDS WERE COLLECTED DIRECTLY FROM UM11490 (pg 149)&lt;/P&gt;&lt;P&gt;# RESET&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0003&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x03, ocf 0x0003, plen 0&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 03 0C 00&lt;/P&gt;&lt;P&gt;# ENABLE SCAN&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x001a 0x3&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x03, ocf 0x001a, plen 1&lt;BR /&gt;03&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 1A 0C 00&lt;/P&gt;&lt;P&gt;# ENABLE EVENT FILTER&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0005 0x02 0x00 0x02&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x03, ocf 0x0005, plen 3&lt;BR /&gt;02 00 02&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 05 0C 00&lt;/P&gt;&lt;P&gt;# ENTER IN TEST MODE&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x06 0x0003&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x06, ocf 0x0003, plen 0&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 03 18 00&lt;/P&gt;&lt;P&gt;# START THE TX TRANSMISSION&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0x01 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x3f, ocf 0x0019, plen 18&lt;BR /&gt;80 80 80 80 01 00 01 01 0D 03 0F 00 00 00 00 00 00 04&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 19 FC 00&lt;/P&gt;&lt;P&gt;# STOP THE TX TRANSMISSION&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xF&lt;BR /&gt;F 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x3f, ocf 0x0019, plen 18&lt;BR /&gt;80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 00 04&lt;BR /&gt;&amp;gt; HCI Event: 0xff plen 6&lt;BR /&gt;19 01 39 00 00 00&lt;/P&gt;&lt;P&gt;-------------------- STOPPING THE SCAN FOR BLE AND CLASSIC BEFORE THE TX TRANSMISSION ----------------&lt;BR /&gt;# RESET&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0003&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x03, ocf 0x0003, plen 0&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 03 0C 00&lt;/P&gt;&lt;P&gt;# ENABLE SCAN&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x001a 0x3&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x03, ocf 0x001a, plen 1&lt;BR /&gt;03&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 1A 0C 00&lt;/P&gt;&lt;P&gt;# ENABLE EVENT FILTER&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0005 0x02 0x00 0x02&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x03, ocf 0x0005, plen 3&lt;BR /&gt;02 00 02&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 05 0C 00&lt;/P&gt;&lt;P&gt;# ENTER IN TEST MODE&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x06 0x0003&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x06, ocf 0x0003, plen 0&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 03 18 00&lt;/P&gt;&lt;P&gt;# DISABLE THE BLE SCAN&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x001a 0x0&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x03, ocf 0x001a, plen 1&lt;BR /&gt;00&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 1A 0C 00&lt;/P&gt;&lt;P&gt;# DISABLE THE CLASSIC SCAN&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x08 0x000C 0x00 0x00&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x08, ocf 0x000c, plen 2&lt;BR /&gt;00 00&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 0C 20 00&lt;/P&gt;&lt;P&gt;# START THE TX TRANSMISSION&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0x01 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x3f, ocf 0x0019, plen 18&lt;BR /&gt;80 80 80 80 01 00 01 01 0D 03 0F 00 00 00 00 00 00 04&lt;BR /&gt;&amp;gt; HCI Event: 0x0e plen 4&lt;BR /&gt;01 19 FC 00&lt;/P&gt;&lt;P&gt;# STOP THE TX TRANSMISSION&lt;BR /&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xFF 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x3f, ocf 0x0019, plen 18&lt;BR /&gt;80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 00 04&lt;BR /&gt;&amp;gt; HCI Event: 0xff plen 6&lt;BR /&gt;19 01 63 07 00 00&lt;/P&gt;&lt;P&gt;** When disabling the scan before entering in the test mode, the stop for TX transmission give us:&lt;/P&gt;&lt;P&gt;root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xFF 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04&lt;BR /&gt;&amp;lt; HCI Command: ogf 0x3f, ocf 0x0019, plen 18&lt;BR /&gt;80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 00 04&lt;BR /&gt;&amp;gt; HCI Event: 0xff plen 6&lt;BR /&gt;19 01 ED 04 00 00&lt;/P&gt;&lt;P&gt;For Wifi 5 GHz&lt;BR /&gt;--------------------------------------------------------------------------------&lt;BR /&gt;Paramters: Continuous transmit, BW = 40 MHz, 802.11ac, No DFS, CH = 40, MCS0 (13.5), Power = 14 dBm&lt;/P&gt;&lt;P&gt;root@oaslv:/home/hexagon# cat /proc/mwlan/adapter0/config&lt;BR /&gt;hardware_status=0&lt;BR /&gt;netlink_num=31&lt;BR /&gt;drv_mode=7&lt;BR /&gt;hssetpara=7,0xff,200,400&lt;BR /&gt;sdcmd52rw=0 0x0 0x00&lt;BR /&gt;rf_test_mode=1&lt;BR /&gt;tx_antenna=1&lt;BR /&gt;rx_antenna=1&lt;BR /&gt;band=1&lt;BR /&gt;bw=1&lt;BR /&gt;channel=44&lt;BR /&gt;radio_mode[0]=3&lt;BR /&gt;radio_mode[1]=&lt;BR /&gt;total rx pkt count=0&lt;BR /&gt;rx multicast/broadcast pkt count=0&lt;BR /&gt;rx fcs error pkt count=0&lt;BR /&gt;tx_power=14 2 0&lt;BR /&gt;tx_continuous=0&lt;BR /&gt;tx_frame=1 4352 0xaaa 1024 1 20 4294967295 0 0 4294967295 0 0 0 -1 -1 -1 -1 -1 -1 -1 05:43:3f:c4:51:ff&lt;BR /&gt;he_tb_tx=0&lt;BR /&gt;trigger_frame=0&lt;BR /&gt;otp_mac_add_rd_wr= 00:00:00:00:00:00&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jul 2026 17:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/IW612-Bluetooth-RF-Test/m-p/2396468#M32933</guid>
      <dc:creator>HelbertPaulino</dc:creator>
      <dc:date>2026-07-17T17:42:22Z</dc:date>
    </item>
  </channel>
</rss>