<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: MC33774 Daisy Chain Dual Loop Connection</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MC33774-Daisy-Chain-Dual-Loop-Connection/m-p/2387884#M32748</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;According to the AN13910 TPL Loopback Recommendation, when two MC33665A TPL ports are connected as a loopback ring, there are several configuration requirements that may cause the behavior you are seeing.&lt;BR /&gt;For a loopback configuration:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;We recommend assigning device addresses (DADD) in ascending order from one side of the ring and in reverse order from the loopback side (I do not see this in your image).&lt;/LI&gt;
&lt;LI&gt;If two ports are connected as loopback, one of the ports should have SYS_PORTx_CFG[RX] = 0 to avoid duplicate data entering the MC33665 buffer.&lt;/LI&gt;
&lt;LI&gt;In addition, one of the ports should have SYS_PORTx_CFG[ALLCHAINS] = 0. If both loopback ports accept ALLCHAINS commands, document states that this can cause signal conflicts and communication errors.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Could you please share the values of SYS_PORT0_CFG and SYS_PORT1_CFG (especially EN, RX, ALLCHAINS, MADD, and CADD)? That would help determine whether the loopback ports are configured according to the AN13910 recommendations.&lt;/P&gt;</description>
    <pubDate>Mon, 29 Jun 2026 18:46:45 GMT</pubDate>
    <dc:creator>ErikaC</dc:creator>
    <dc:date>2026-06-29T18:46:45Z</dc:date>
    <item>
      <title>MC33774 Daisy Chain Dual Loop Connection</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MC33774-Daisy-Chain-Dual-Loop-Connection/m-p/2387695#M32743</link>
      <description>&lt;P&gt;HI.&lt;/P&gt;
&lt;P&gt;我当前使用MC33665A+MC33774的AFE采样系统组成双链回环的结构，配置MC33665A的PORT0和PORT1分别为MADD0和MADD1，当前发送所有指令均由MADD0发送。当我只连接PORT0到DC1之间的菊花链时，我的通讯都是正常的，但是当我把PORT1和DC2之间的菊花链也连接后，我再去请求33774发现33774无法回复响应帧，这是为什么？我回读确认过33665的PORT端口配置没有错误，并且将33774中的SYS_TPL_CFG.RESPCFG设置为00 SAME模式。&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;I am currently using an AFE sampling system consisting of the MC33665A + MC33774 in a dual-ring loop configuration. I have configured PORT0 and PORT1 of the MC33665A as MADD0 and MADD1, respectively, and all commands are currently sent through MADD0.&lt;/P&gt;
&lt;P&gt;When I connect only the daisy chain between PORT0 and DC1, communication works correctly. However, after I also connect the daisy chain between PORT1 and DC2, the MC33774 no longer responds when I send requests to it.&lt;/P&gt;
&lt;P&gt;Why does this happen?&lt;/P&gt;
&lt;P&gt;I have read back and verified that the MC33665 PORT configuration is correct, and I have configured SYS_TPL_CFG.RESPCFG = 00 (SAME mode) in the MC33774.&lt;/P&gt;
&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Embedded_novice_0-1782728020846.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/390576i164ED2A8580F30E1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Embedded_novice_0-1782728020846.png" alt="Embedded_novice_0-1782728020846.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jun 2026 18:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MC33774-Daisy-Chain-Dual-Loop-Connection/m-p/2387695#M32743</guid>
      <dc:creator>Embedded_novice</dc:creator>
      <dc:date>2026-06-29T18:26:29Z</dc:date>
    </item>
    <item>
      <title>Re: MC33774 Daisy Chain Dual Loop Connection</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MC33774-Daisy-Chain-Dual-Loop-Connection/m-p/2387884#M32748</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;According to the AN13910 TPL Loopback Recommendation, when two MC33665A TPL ports are connected as a loopback ring, there are several configuration requirements that may cause the behavior you are seeing.&lt;BR /&gt;For a loopback configuration:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;We recommend assigning device addresses (DADD) in ascending order from one side of the ring and in reverse order from the loopback side (I do not see this in your image).&lt;/LI&gt;
&lt;LI&gt;If two ports are connected as loopback, one of the ports should have SYS_PORTx_CFG[RX] = 0 to avoid duplicate data entering the MC33665 buffer.&lt;/LI&gt;
&lt;LI&gt;In addition, one of the ports should have SYS_PORTx_CFG[ALLCHAINS] = 0. If both loopback ports accept ALLCHAINS commands, document states that this can cause signal conflicts and communication errors.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Could you please share the values of SYS_PORT0_CFG and SYS_PORT1_CFG (especially EN, RX, ALLCHAINS, MADD, and CADD)? That would help determine whether the loopback ports are configured according to the AN13910 recommendations.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jun 2026 18:46:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MC33774-Daisy-Chain-Dual-Loop-Connection/m-p/2387884#M32748</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2026-06-29T18:46:45Z</dc:date>
    </item>
    <item>
      <title>Re: MC33774 Daisy Chain Dual Loop Connection</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MC33774-Daisy-Chain-Dual-Loop-Connection/m-p/2388005#M32756</link>
      <description>&lt;P&gt;HI.&lt;/P&gt;&lt;P&gt;1.我想知道从MADD=1的位置反向分配DADD是必须的吗？&lt;/P&gt;&lt;P&gt;2.我当前的SYS_PORT0_CFG配置为TIMEOUT=0,CADD=1,MADD=0,PROTOCOL=1,ALLCHAINS=1,TERM=1,RX=1,EN=1&lt;/P&gt;&lt;P&gt;SYS_PORT1_CFG配置为TIMEOUT=0,CADD=1,MADD=1,PROTOCOL=1,ALLCHAINS=1,TERM=1,RX=1,EN=1&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jun 2026 02:58:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MC33774-Daisy-Chain-Dual-Loop-Connection/m-p/2388005#M32756</guid>
      <dc:creator>Embedded_novice</dc:creator>
      <dc:date>2026-06-30T02:58:29Z</dc:date>
    </item>
    <item>
      <title>Re: MC33774 Daisy Chain Dual Loop Connection</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MC33774-Daisy-Chain-Dual-Loop-Connection/m-p/2388581#M32769</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;According to AN13910 TPL Loopback Recommendation, the DADD assignment should be reversed from the MADD=1 side in a loopback topology.&lt;/P&gt;
&lt;P&gt;In addition, your current configuration has RX=1 and ALLCHAINS=1 on both ports. For a loopback connection, we recommend disabling RX and ALLCHAINS on one of the ports to avoid duplicate routing and communication conflicts.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please try configuring one port with RX=0 and ALLCHAINS=0 (for example, PORT1) and verify whether the MC33774 starts returning response frames?&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jun 2026 18:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MC33774-Daisy-Chain-Dual-Loop-Connection/m-p/2388581#M32769</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2026-06-30T18:56:39Z</dc:date>
    </item>
  </channel>
</rss>