<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 PN7160 (B1) not initializing (SPI)</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PN7160-B1-not-initializing-SPI/m-p/2372249#M32305</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a PN7160 eval board (OM27160B1HN) that I am using with an ESP32.&amp;nbsp;&lt;SPAN&gt;I adapted the NXP-NCI2.0 LPC55S6x MIRAFE example for the ESP. I also reviewed it according to the UM11495 and I also took a look on the "&lt;SPAN&gt;Migration Guide of NXP-NCI 2.0 SPI examples"&lt;/SPAN&gt;. However, I cannot properly complete the initialization. After toggling the VEN pin for the hard reset, I send a NCI CORE RESET message, but I get no reply from the PN7160 (the IRQ never triggers after the message). The only alive indication I see from the PN7160 is that when the VEN is low (during the hard reset) the IRQ pin goes high. The MOSI, CLK and NSS signals seem fine as well &lt;SPAN&gt;on the oscilloscope. Voltages on the VDD and VBAT are 3.28V&lt;/SPAN&gt;. I configured the SPI for 500kHz.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What could be the issue?&lt;/SPAN&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;PS.: I attached one oscilloscope image from the &lt;SPAN&gt;CORE RESET message&lt;/SPAN&gt;. The signals are: yellow (MOSI), cyan (MISO), purple (NSS) and blue (CLK). At this image I was trying the mode 3 on the SPI config - CPOL 1 (High) and CPHAL 1 (Trailing Edge). I tried all the 4 modes, but none of them worked.&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Thu, 28 May 2026 06:38:27 GMT</pubDate>
    <dc:creator>Magnetuz</dc:creator>
    <dc:date>2026-05-28T06:38:27Z</dc:date>
    <item>
      <title>PN7160 (B1) not initializing (SPI)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7160-B1-not-initializing-SPI/m-p/2372249#M32305</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a PN7160 eval board (OM27160B1HN) that I am using with an ESP32.&amp;nbsp;&lt;SPAN&gt;I adapted the NXP-NCI2.0 LPC55S6x MIRAFE example for the ESP. I also reviewed it according to the UM11495 and I also took a look on the "&lt;SPAN&gt;Migration Guide of NXP-NCI 2.0 SPI examples"&lt;/SPAN&gt;. However, I cannot properly complete the initialization. After toggling the VEN pin for the hard reset, I send a NCI CORE RESET message, but I get no reply from the PN7160 (the IRQ never triggers after the message). The only alive indication I see from the PN7160 is that when the VEN is low (during the hard reset) the IRQ pin goes high. The MOSI, CLK and NSS signals seem fine as well &lt;SPAN&gt;on the oscilloscope. Voltages on the VDD and VBAT are 3.28V&lt;/SPAN&gt;. I configured the SPI for 500kHz.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What could be the issue?&lt;/SPAN&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;PS.: I attached one oscilloscope image from the &lt;SPAN&gt;CORE RESET message&lt;/SPAN&gt;. The signals are: yellow (MOSI), cyan (MISO), purple (NSS) and blue (CLK). At this image I was trying the mode 3 on the SPI config - CPOL 1 (High) and CPHAL 1 (Trailing Edge). I tried all the 4 modes, but none of them worked.&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 28 May 2026 06:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7160-B1-not-initializing-SPI/m-p/2372249#M32305</guid>
      <dc:creator>Magnetuz</dc:creator>
      <dc:date>2026-05-28T06:38:27Z</dc:date>
    </item>
    <item>
      <title>Re: PN7160 (B1) not initializing (SPI)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7160-B1-not-initializing-SPI/m-p/2374602#M32418</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263214"&gt;@Magnetuz&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;My apologies, please consider that implementation and porting to third-party platforms is out of our support scope and must be done entirely by the customer.&lt;/P&gt;
&lt;P&gt;According to &lt;A href="https://www.nxp.com/docs/en/data-sheet/PN7160_PN7161.pdf" target="_blank"&gt;PN7160&lt;/A&gt;, Section 11.2.2.2, CPOL/CPHA are set as follows:&lt;/P&gt;
&lt;P&gt;- CPHA = 0: data are sampled on MOSI on the odd clock edges of SCK after NSS goes low.&lt;BR /&gt;- CPOL = 0: the clock is idle low and the first valid edge of SCK will be a rising one.&lt;/P&gt;
&lt;P&gt;Also, please consider connecting VBAT to 5V.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 01 Jun 2026 21:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7160-B1-not-initializing-SPI/m-p/2374602#M32418</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-06-01T21:19:09Z</dc:date>
    </item>
  </channel>
</rss>