<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Kernel crash while untar the rootfs after bootup</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Kernel-crash-while-untar-the-rootfs-after-bootup/m-p/2347000#M31529</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I have created four partitions on my i.MX8MP board. The first partition contains the kernel Image and other DTB files. The next two partitions are used for the root filesystem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After booting the device, I update the root filesystem using the following commands:&lt;/SPAN&gt;&lt;BR /&gt;the Current mount partition is&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;mmcblk2p2.i just untar the file. i am running QT also.without QT it is working fine i am able to untar.But with QT package it gone to crash.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN&gt;mount /dev/mmcblk2p3 p3&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;tar -xvf rootfs.tar -C p3&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sometimes the update works correctly, but other times the kernel crashes.I have 4 GB RAM. i have attached Log.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;****-----------------------------*****&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/sync&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/sysctl&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/syslogd&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/tac&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/tail&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/tar&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/[ 88.650509] Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.661042] Modules linked in:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.664100] CPU: 3 UID: 0 PID: 316 Comm: swupdate-progre Not tainted 6.12.49-lts-next-ga2ae9d0ae881 #1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.673408] Hardware name: NXP i.MX8MPlus EVK board (DT)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.678718] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.685682] pc : task_fpsimd_load+0xa4/0x208&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.689959] lr : fpsimd_restore_current_state+0xa8/0xc8&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.695188] sp : ffff8000847e3e30&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.698500] x29: ffff8000847e3e30 x28: ffff0000d500b300 x27: 0000000000000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.705643] x26: 0000000000000000 x25: 0000000000000000 x24: 0000000000000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.712785] x23: 0000000080000000 x22: 0000000000000020 x21: ffff8000847e3eb0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.719927] x20: ffff0000d500b300 x19: 000000000000020c x18: ffff800082a95400&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.727066] x17: 0000000000000060 x16: 0000000000000018 x15: 0000000000010000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.734208] x14: 000000000001e000 x13: ffff0000d500b380 x12: 0000000000000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.741348] x11: 00000000000000c0 x10: 0000000000000a70 x9 : ffff8000847e3c00&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.748493] x8 : ffff0000d500bdd0 x7 : 0000000000000000 x6 : 0000000000400100&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.755634] x5 : 0000000000000020 x4 : 0000000000000000 x3 : 0000000000000200&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.762775] x2 : 0000000000000008 x1 : 0000000000000208 x0 : 0000000000000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.769917] Call trace:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.772362] task_fpsimd_load+0xa4/0x208&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.776286] fpsimd_restore_current_state+0xa8/0xc8&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.781167] do_notify_resume+0xc4/0x148&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.785090] el0_svc+0xd4/0x100&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.788234] el0t_64_sync_handler+0x120/0x12c&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.792591] el0t_64_sync+0x190/0x194&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.796259] Code: d5384101 f9457821 00000000 00000000 (00000000)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.802355] ---[ end trace 0000000000000000 ]---&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.806974] Kernel panic - not syncing: Oops - Undefined instruction: Fatal exception in interrupt&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.815931] SMP: stopping secondary CPUs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 89.819855] SMP: failed to stop secondary CPUs 0,2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 89.824649] Kernel Offset: disabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 89.828134] CPU features: 0x00,00000080,00200000,4200420b&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 89.833534] Memory Limit: none&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 89.836589] ---[ end Kernel panic - not syncing: Oops - Undefined instruction: Fatal exception in interrupt ]---&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 08 Apr 2026 10:01:57 GMT</pubDate>
    <dc:creator>ManikandanRama</dc:creator>
    <dc:date>2026-04-08T10:01:57Z</dc:date>
    <item>
      <title>Kernel crash while untar the rootfs after bootup</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Kernel-crash-while-untar-the-rootfs-after-bootup/m-p/2347000#M31529</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I have created four partitions on my i.MX8MP board. The first partition contains the kernel Image and other DTB files. The next two partitions are used for the root filesystem.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After booting the device, I update the root filesystem using the following commands:&lt;/SPAN&gt;&lt;BR /&gt;the Current mount partition is&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;mmcblk2p2.i just untar the file. i am running QT also.without QT it is working fine i am able to untar.But with QT package it gone to crash.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;SPAN&gt;mount /dev/mmcblk2p3 p3&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;tar -xvf rootfs.tar -C p3&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Sometimes the update works correctly, but other times the kernel crashes.I have 4 GB RAM. i have attached Log.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;****-----------------------------*****&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/sync&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/sysctl&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/syslogd&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/tac&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/tail&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/alternatives/tar&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;./usr/lib/opkg/[ 88.650509] Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.661042] Modules linked in:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.664100] CPU: 3 UID: 0 PID: 316 Comm: swupdate-progre Not tainted 6.12.49-lts-next-ga2ae9d0ae881 #1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.673408] Hardware name: NXP i.MX8MPlus EVK board (DT)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.678718] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.685682] pc : task_fpsimd_load+0xa4/0x208&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.689959] lr : fpsimd_restore_current_state+0xa8/0xc8&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.695188] sp : ffff8000847e3e30&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.698500] x29: ffff8000847e3e30 x28: ffff0000d500b300 x27: 0000000000000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.705643] x26: 0000000000000000 x25: 0000000000000000 x24: 0000000000000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.712785] x23: 0000000080000000 x22: 0000000000000020 x21: ffff8000847e3eb0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.719927] x20: ffff0000d500b300 x19: 000000000000020c x18: ffff800082a95400&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.727066] x17: 0000000000000060 x16: 0000000000000018 x15: 0000000000010000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.734208] x14: 000000000001e000 x13: ffff0000d500b380 x12: 0000000000000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.741348] x11: 00000000000000c0 x10: 0000000000000a70 x9 : ffff8000847e3c00&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.748493] x8 : ffff0000d500bdd0 x7 : 0000000000000000 x6 : 0000000000400100&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.755634] x5 : 0000000000000020 x4 : 0000000000000000 x3 : 0000000000000200&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.762775] x2 : 0000000000000008 x1 : 0000000000000208 x0 : 0000000000000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.769917] Call trace:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.772362] task_fpsimd_load+0xa4/0x208&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.776286] fpsimd_restore_current_state+0xa8/0xc8&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.781167] do_notify_resume+0xc4/0x148&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.785090] el0_svc+0xd4/0x100&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.788234] el0t_64_sync_handler+0x120/0x12c&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.792591] el0t_64_sync+0x190/0x194&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.796259] Code: d5384101 f9457821 00000000 00000000 (00000000)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.802355] ---[ end trace 0000000000000000 ]---&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.806974] Kernel panic - not syncing: Oops - Undefined instruction: Fatal exception in interrupt&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 88.815931] SMP: stopping secondary CPUs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 89.819855] SMP: failed to stop secondary CPUs 0,2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 89.824649] Kernel Offset: disabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 89.828134] CPU features: 0x00,00000080,00200000,4200420b&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 89.833534] Memory Limit: none&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 89.836589] ---[ end Kernel panic - not syncing: Oops - Undefined instruction: Fatal exception in interrupt ]---&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Apr 2026 10:01:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Kernel-crash-while-untar-the-rootfs-after-bootup/m-p/2347000#M31529</guid>
      <dc:creator>ManikandanRama</dc:creator>
      <dc:date>2026-04-08T10:01:57Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel crash while untar the rootfs after bootup</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Kernel-crash-while-untar-the-rootfs-after-bootup/m-p/2348565#M31549</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261190"&gt;@ManikandanRama&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;Could you please share how you are partitioning your SD card/eMMC?&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;I recommend following the instructions in Chapter 4.3 of our &lt;A href="https://www.nxp.com/docs/en/user-guide/UG10163.pdf" target="_self"&gt;Linux User Guide&lt;/A&gt; to ensure your system is flashed correctly.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Thu, 09 Apr 2026 16:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Kernel-crash-while-untar-the-rootfs-after-bootup/m-p/2348565#M31549</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2026-04-09T16:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel crash while untar the rootfs after bootup</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Kernel-crash-while-untar-the-rootfs-after-bootup/m-p/2348959#M31556</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206761"&gt;@Chavira&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I am using a &lt;STRONG&gt;16 GB eMMC&lt;/STRONG&gt;, and I have created partitions using a .wks file as shown below:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;part u-boot --source rawcopy --sourceparams="file=imx-boot.tagged" --ondisk mmcblk --no-table --align 33&lt;/P&gt;&lt;P&gt;# Boot (128MB)&lt;BR /&gt;part /boot --source bootimg-partition --ondisk mmcblk --fstype=vfat --label boot --active --align 8192 --fixed-size 128&lt;/P&gt;&lt;P&gt;# RootFS A (3GB)&lt;BR /&gt;part / --source rootfs --ondisk mmcblk --fstype=ext4 --label rootfsA --align 8192 --size 3072&lt;/P&gt;&lt;P&gt;# RootFS B (3GB)&lt;BR /&gt;part / --source rootfs --ondisk mmcblk --fstype=ext4 --label rootfsB --align 8192 --size 3072&lt;/P&gt;&lt;P&gt;# Recovery (500MB)&lt;BR /&gt;part /recovery --ondisk mmcblk --fstype=ext4 --label recovery --align 8192 --fixed-size 500&lt;/P&gt;&lt;P&gt;bootloader --ptable msdos&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently, the system is running from &lt;STRONG&gt;Partition 2 (rootfsA)&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;To update a new root filesystem image, I am using the following steps:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;mkdir p3&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;mount /dev/mmcblk2p3 p3&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;tar -xvf rootfs.tar -C p3&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;in that time i am getting this issue.i am using 2 GB RAM with QT application.is there any dts or kernel changes are needed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 10 Apr 2026 07:02:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Kernel-crash-while-untar-the-rootfs-after-bootup/m-p/2348959#M31556</guid>
      <dc:creator>ManikandanRama</dc:creator>
      <dc:date>2026-04-10T07:02:13Z</dc:date>
    </item>
  </channel>
</rss>