<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic îmx8 container encryption in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/%C3%AEmx8-container-encryption/m-p/2345162#M31474</link>
    <description>&lt;P&gt;so i read the docs guide to encrypt the container&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2025.04/doc/imx/ahab/guides/mx8_mx8x_encrypted_boot.txt" target="_blank"&gt;https://github.com/nxp-imx/uboot-imx/blob/lf_v2025.04/doc/imx/ahab/guides/mx8_mx8x_encrypted_boot.txt&lt;/A&gt;&lt;/P&gt;&lt;P&gt;but the problem is with enabling encrypted boot support,the cst tool 4.0.1 provided by nxp dosent have a code folder that contains backend ... so do i need the cst source code to compile the tool and enable encryption support?and if so from where i download the source code since i have only the cst 4.0.1 and it dosent contain container encryption support&lt;/P&gt;</description>
    <pubDate>Fri, 03 Apr 2026 22:01:18 GMT</pubDate>
    <dc:creator>anas-8888</dc:creator>
    <dc:date>2026-04-03T22:01:18Z</dc:date>
    <item>
      <title>îmx8 container encryption</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/%C3%AEmx8-container-encryption/m-p/2345162#M31474</link>
      <description>&lt;P&gt;so i read the docs guide to encrypt the container&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-imx/uboot-imx/blob/lf_v2025.04/doc/imx/ahab/guides/mx8_mx8x_encrypted_boot.txt" target="_blank"&gt;https://github.com/nxp-imx/uboot-imx/blob/lf_v2025.04/doc/imx/ahab/guides/mx8_mx8x_encrypted_boot.txt&lt;/A&gt;&lt;/P&gt;&lt;P&gt;but the problem is with enabling encrypted boot support,the cst tool 4.0.1 provided by nxp dosent have a code folder that contains backend ... so do i need the cst source code to compile the tool and enable encryption support?and if so from where i download the source code since i have only the cst 4.0.1 and it dosent contain container encryption support&lt;/P&gt;</description>
      <pubDate>Fri, 03 Apr 2026 22:01:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/%C3%AEmx8-container-encryption/m-p/2345162#M31474</guid>
      <dc:creator>anas-8888</dc:creator>
      <dc:date>2026-04-03T22:01:18Z</dc:date>
    </item>
    <item>
      <title>Re: îmx8 container encryption</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/%C3%AEmx8-container-encryption/m-p/2346573#M31513</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Seems that the documentation is a bit old, please note that this step is no longer needed in CST after version 3.0.0&lt;BR /&gt;&lt;BR /&gt;Also, this App note is more up to date for encrypt boot:&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13994" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=AN13994&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;And there is the SPSDK as well:&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/secure-provisioning-sdk-spsdk:SPSDK" target="_blank"&gt;https://www.nxp.com/design/design-center/software/development-software/secure-provisioning-sdk-spsdk:SPSDK&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Apr 2026 22:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/%C3%AEmx8-container-encryption/m-p/2346573#M31513</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2026-04-07T22:47:07Z</dc:date>
    </item>
  </channel>
</rss>