<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックTJA1121: Difference between DEVICE_CONTROL_START_OPERATION and PHY_CONTROL_START_OPERATION</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1121-Difference-between-DEVICE-CONTROL-START-OPERATION-and/m-p/2336767#M31355</link>
    <description>&lt;P&gt;From the TJA1121 AN4517, the last step of PHY initialization is DEVICE_CONTROL_START_OPERATION=1.&amp;nbsp; However, the demo code didn't write to 0x40 but instead write to register 0x8100 (PHY_CONTROL) to start PHY operation.&amp;nbsp; What's the difference between the two registers?&amp;nbsp; Now the PHY_STATUS MM30.0x810C=0x10A (i.e. link is in sync state but Transmit state is SEND_Z).&amp;nbsp; &amp;nbsp;But the same code on EVK works fine.&amp;nbsp; Why the transmitter state is SEND_Z?&amp;nbsp; What debug steps do you suggest?&amp;nbsp; Thanks.&lt;/P&gt;&lt;P&gt;Config:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Config6=open: autonomous lead&lt;/LI&gt;&lt;LI&gt;I haven't started data transfer from MCU to TJA1121 via SGMII yet&lt;/LI&gt;&lt;LI&gt;Device confirmed not in reset (via reset pin) or low power mode (8181h is 0x0000)&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Fri, 20 Mar 2026 17:15:06 GMT</pubDate>
    <dc:creator>peter123</dc:creator>
    <dc:date>2026-03-20T17:15:06Z</dc:date>
    <item>
      <title>TJA1121: Difference between DEVICE_CONTROL_START_OPERATION and PHY_CONTROL_START_OPERATION</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1121-Difference-between-DEVICE-CONTROL-START-OPERATION-and/m-p/2336767#M31355</link>
      <description>&lt;P&gt;From the TJA1121 AN4517, the last step of PHY initialization is DEVICE_CONTROL_START_OPERATION=1.&amp;nbsp; However, the demo code didn't write to 0x40 but instead write to register 0x8100 (PHY_CONTROL) to start PHY operation.&amp;nbsp; What's the difference between the two registers?&amp;nbsp; Now the PHY_STATUS MM30.0x810C=0x10A (i.e. link is in sync state but Transmit state is SEND_Z).&amp;nbsp; &amp;nbsp;But the same code on EVK works fine.&amp;nbsp; Why the transmitter state is SEND_Z?&amp;nbsp; What debug steps do you suggest?&amp;nbsp; Thanks.&lt;/P&gt;&lt;P&gt;Config:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Config6=open: autonomous lead&lt;/LI&gt;&lt;LI&gt;I haven't started data transfer from MCU to TJA1121 via SGMII yet&lt;/LI&gt;&lt;LI&gt;Device confirmed not in reset (via reset pin) or low power mode (8181h is 0x0000)&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Fri, 20 Mar 2026 17:15:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1121-Difference-between-DEVICE-CONTROL-START-OPERATION-and/m-p/2336767#M31355</guid>
      <dc:creator>peter123</dc:creator>
      <dc:date>2026-03-20T17:15:06Z</dc:date>
    </item>
  </channel>
</rss>