<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: SC18IS606 - how to read and write in Python</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IS606-how-to-read-and-write-in-Python/m-p/2331504#M31323</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;We do not provide an official Python library specifically for SC18IS606, but the device uses a very simple command‑based protocol, so it is pretty straightforward to access using any standard Python I²C package.&lt;/P&gt;
&lt;P&gt;To understand how to send commands to the SC18IS606, I recommend to look at:&lt;/P&gt;
&lt;P&gt;Chapter 8 – “I²C‑bus to SPI communications example” in the SC18IS606 datasheet which shows complete I²C command sequences for SPI reads/writes.&lt;/P&gt;
&lt;P&gt;UM11666 – SC18IS606-EVB board examples (section 4.4) contains sequences for configuring SPI, reading device ID, EEPROM read/write etc.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Thu, 12 Mar 2026 13:11:05 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2026-03-12T13:11:05Z</dc:date>
    <item>
      <title>SC18IS606 - how to read and write in Python</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IS606-how-to-read-and-write-in-Python/m-p/2331457#M31322</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using SC18IS606 to read PT1000 temperature sensor through&amp;nbsp;&lt;SPAN&gt;MAX31865 having SPI interface. We need to connect&amp;nbsp;SC18IS606 to I2C master MCP2221. Do we have Python libraries for&amp;nbsp;SC18IS606 and Python example how to read and write to&amp;nbsp;SC18IS606 ?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Mar 2026 11:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IS606-how-to-read-and-write-in-Python/m-p/2331457#M31322</guid>
      <dc:creator>johnpeter</dc:creator>
      <dc:date>2026-03-12T11:44:10Z</dc:date>
    </item>
    <item>
      <title>Re: SC18IS606 - how to read and write in Python</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IS606-how-to-read-and-write-in-Python/m-p/2331504#M31323</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;We do not provide an official Python library specifically for SC18IS606, but the device uses a very simple command‑based protocol, so it is pretty straightforward to access using any standard Python I²C package.&lt;/P&gt;
&lt;P&gt;To understand how to send commands to the SC18IS606, I recommend to look at:&lt;/P&gt;
&lt;P&gt;Chapter 8 – “I²C‑bus to SPI communications example” in the SC18IS606 datasheet which shows complete I²C command sequences for SPI reads/writes.&lt;/P&gt;
&lt;P&gt;UM11666 – SC18IS606-EVB board examples (section 4.4) contains sequences for configuring SPI, reading device ID, EEPROM read/write etc.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Thu, 12 Mar 2026 13:11:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IS606-how-to-read-and-write-in-Python/m-p/2331504#M31323</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2026-03-12T13:11:05Z</dc:date>
    </item>
  </channel>
</rss>