<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: A5M36TG140_Biasing Sequence in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/A5M36TG140-Biasing-Sequence/m-p/2304299#M31135</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thank you for your suppor.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;</description>
    <pubDate>Sun, 01 Feb 2026 11:10:19 GMT</pubDate>
    <dc:creator>joshlim</dc:creator>
    <dc:date>2026-02-01T11:10:19Z</dc:date>
    <item>
      <title>A5M36TG140_Biasing Sequence</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/A5M36TG140-Biasing-Sequence/m-p/2297641#M31080</link>
      <description>&lt;P&gt;I am writing to inquire about a product-related matter that we would like to clarify.&lt;/P&gt;&lt;P&gt;According to the datasheet (page 7), under the Correct Biasing Sequence – Turn ON section, the following sequence is described:&lt;/P&gt;&lt;P&gt;GaN TR bias setting&lt;BR /&gt;LDMOS bias setting&lt;/P&gt;&lt;P&gt;However, our current biasing sequence is as follows:&lt;BR /&gt;LDMOS bias setting (80 mA / 40 mA)&lt;BR /&gt;GaN peaking voltage setting&lt;BR /&gt;Apply 50 V and then set GaN carrier bias&lt;BR /&gt;Apply RF signal&lt;/P&gt;&lt;P&gt;We would like to ask the manufacturer whether this biasing sequence could potentially have any impact on GaN TR reliability or damage.&lt;/P&gt;&lt;P&gt;Your confirmation would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jan 2026 23:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/A5M36TG140-Biasing-Sequence/m-p/2297641#M31080</guid>
      <dc:creator>joshlim</dc:creator>
      <dc:date>2026-01-21T23:52:40Z</dc:date>
    </item>
    <item>
      <title>Re: A5M36TG140_Biasing Sequence</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/A5M36TG140-Biasing-Sequence/m-p/2298511#M31094</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;
&lt;P&gt;The proposed biasing sequence applies the GaN drain voltage before explicitly turning the GaN gate fully off.&lt;BR /&gt;This approach may work in systems that include additional hardware protection, but it is not the sequence recommended in the A5M36TG140 datasheet.&lt;BR /&gt;The sequence described in the datasheet ensures that the GaN device is completely turned off before any high drain voltage is applied. This helps prevent unintended drain current, reduces electrical stress, and protects the device from long‑term damage.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Any biasing or de‑biasing sequence that differs from the datasheet recommendation is outside the specified operating conditions and must be carefully reviewed and validated at the system level, since correct operation and long‑term reliability are not guaranteed.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jan 2026 17:23:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/A5M36TG140-Biasing-Sequence/m-p/2298511#M31094</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2026-01-22T17:23:08Z</dc:date>
    </item>
    <item>
      <title>Re: A5M36TG140_Biasing Sequence</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/A5M36TG140-Biasing-Sequence/m-p/2304299#M31135</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thank you for your suppor.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;</description>
      <pubDate>Sun, 01 Feb 2026 11:10:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/A5M36TG140-Biasing-Sequence/m-p/2304299#M31135</guid>
      <dc:creator>joshlim</dc:creator>
      <dc:date>2026-02-01T11:10:19Z</dc:date>
    </item>
  </channel>
</rss>