<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: 有关TJA1145T/FD休眠唤醒问题</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/%E6%9C%89%E5%85%B3TJA1145T-FD%E4%BC%91%E7%9C%A0%E5%94%A4%E9%86%92%E9%97%AE%E9%A2%98/m-p/2267515#M30890</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;To recover without cycling BAT:&lt;BR /&gt;Power up VIO and VCC.&lt;BR /&gt;Read Main Status (check FSMS). If set, re‑configure wake and partial networking.&lt;BR /&gt;Clear event flags (0x61–0x64).&lt;BR /&gt;Set MC=111 (Normal) and enable CAN via CMC=01 or 10.&lt;BR /&gt;Ensure TXD is HIGH and confirm CTS=1 before starting CAN.&lt;/P&gt;
&lt;P&gt;If WAKE is used, it must see a valid edge (e.g. follow KL15). BAT should remain permanently connected.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
    <pubDate>Mon, 22 Dec 2025 08:23:47 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2025-12-22T08:23:47Z</dc:date>
    <item>
      <title>有关TJA1145T/FD休眠唤醒问题</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/%E6%9C%89%E5%85%B3TJA1145T-FD%E4%BC%91%E7%9C%A0%E5%94%A4%E9%86%92%E9%97%AE%E9%A2%98/m-p/2267134#M30876</link>
      <description>&lt;P&gt;1.使用S32K通过SPI配置好normal模式，收发器正常工作&lt;/P&gt;&lt;P&gt;2.检测到KL15电下电，把1145配置为sleep模式，由于不想使用CAN 唤醒方式，所以使能的是WAKE引脚上升沿唤醒，但是WAKE引脚上升沿唤醒WAKE引脚接的是下拉，这期间BAT引脚一直供电&lt;/P&gt;&lt;P&gt;3.成功进入sleep模式后，s32k芯片下电，kl15上电后，s32k正常工作，执行1145配置函数，配置为normal模式，但是发现收发器不能正常工作&lt;/P&gt;&lt;P&gt;只有当bat引脚下电重新上电后，再通过S32K配置才能正常&lt;/P&gt;&lt;P&gt;这个是1145芯片的特性，还是哪里配置的不正确，是否需要WAKE引脚跟随KL15一起上电唤醒，或者BAT引脚跟随KL15状态&lt;/P&gt;</description>
      <pubDate>Sat, 20 Dec 2025 07:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/%E6%9C%89%E5%85%B3TJA1145T-FD%E4%BC%91%E7%9C%A0%E5%94%A4%E9%86%92%E9%97%AE%E9%A2%98/m-p/2267134#M30876</guid>
      <dc:creator>lyq</dc:creator>
      <dc:date>2025-12-20T07:07:45Z</dc:date>
    </item>
    <item>
      <title>Re: 有关TJA1145T/FD休眠唤醒问题</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/%E6%9C%89%E5%85%B3TJA1145T-FD%E4%BC%91%E7%9C%A0%E5%94%A4%E9%86%92%E9%97%AE%E9%A2%98/m-p/2267515#M30890</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;To recover without cycling BAT:&lt;BR /&gt;Power up VIO and VCC.&lt;BR /&gt;Read Main Status (check FSMS). If set, re‑configure wake and partial networking.&lt;BR /&gt;Clear event flags (0x61–0x64).&lt;BR /&gt;Set MC=111 (Normal) and enable CAN via CMC=01 or 10.&lt;BR /&gt;Ensure TXD is HIGH and confirm CTS=1 before starting CAN.&lt;/P&gt;
&lt;P&gt;If WAKE is used, it must see a valid edge (e.g. follow KL15). BAT should remain permanently connected.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 22 Dec 2025 08:23:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/%E6%9C%89%E5%85%B3TJA1145T-FD%E4%BC%91%E7%9C%A0%E5%94%A4%E9%86%92%E9%97%AE%E9%A2%98/m-p/2267515#M30890</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-12-22T08:23:47Z</dc:date>
    </item>
  </channel>
</rss>